Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hi,
Thanks in advance for your help. I tried updating the PM8244 firmware from v4.5.0 to v4.6.0 using ION Setup. The ZIP file includes three templates—I selected the standard one for this model. However, I received an error: Problem programming RMP Framework.
Could you please confirm if the attached firmware files are the latest for this meter?
PM8000 v4.6.0 Firmware and Associated Files | Schneider Electric
Link copied. Please paste this link to share this article on your social media post.
Hello @ABDUL8 ,
Yes V4.6.0 is the latest version of meter firmware and template. Note that a V4.6.0 template cannot be pasted on a V4.5.0 meter. Based on screenshots you will need to upgrade your meter's firmware to V4.6.0 before applying the template.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi @ABDUL8
Yes, the firmware package is correct and includes all components for firmware version V4.6.
PM8243 is a DIN rail-mounted meter with Standard feature set and no display. However based on meter's Serial Number (ME-2502D871-03), it should be PM8244 which is the same as PM8243 but packaged with Remote Display:
As for 'Problem programming RMP framework’, please note that there are two different methods for loading the firmware onto a meter:
Rapid Meter Programming (RMP) – a faster method
Non-RMP
To disable RMP, hold down the ALT key before sending the file to the meter. During the upgrade process, press and hold the ALT key while clicking the Upgrade button. This will disable upgrade throttling/API version, preventing interruptions during template uploading.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Hello @ABDUL8 ,
Yes V4.6.0 is the latest version of meter firmware and template. Note that a V4.6.0 template cannot be pasted on a V4.5.0 meter. Based on screenshots you will need to upgrade your meter's firmware to V4.6.0 before applying the template.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi @ABDUL8
Yes, the firmware package is correct and includes all components for firmware version V4.6.
PM8243 is a DIN rail-mounted meter with Standard feature set and no display. However based on meter's Serial Number (ME-2502D871-03), it should be PM8244 which is the same as PM8243 but packaged with Remote Display:
As for 'Problem programming RMP framework’, please note that there are two different methods for loading the firmware onto a meter:
Rapid Meter Programming (RMP) – a faster method
Non-RMP
To disable RMP, hold down the ALT key before sending the file to the meter. During the upgrade process, press and hold the ALT key while clicking the Upgrade button. This will disable upgrade throttling/API version, preventing interruptions during template uploading.
Best Regards,
-Mehran
L3 Expert Advanced metering
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.