Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8240 Communication Capabilities

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8240 Communication Capabilities
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Gladwin
Gladwin Contributor
Contributor

Posted: ‎2024-08-06 05:06 AM . Last Modified: ‎2024-08-06 05:08 AM

0 Likes
1
1240
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
‎2024-08-06 05:06 AM

PM8240 Communication Capabilities

Hi Team

Please may I ask you to verify if it is possible to simultaneously use the 2 x Ethernet Ports with IEC61850 and also the RS485 Port with Modbus RTU (ie can customer use all three ports simultaneously from different Masters)?  for PM8240.

 

thanks 

Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-08-06 08:22 AM

0 Likes
0
1233
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
‎2024-08-06 08:22 AM

Hello @Gladwin ,

 

Yes it is possible for the meter to use multiple ports at the same time. One item to not is that both Ethernet ports are the same IP and cannot be isolated networks. If you connect 2 different networks the meter will bridge them. Note that meter supports multiple Port connections on 1 Ethernet connection.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Reply 1
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-08-06 08:22 AM

0 Likes
0
1233
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
‎2024-08-06 08:22 AM

Hello @Gladwin ,

 

Yes it is possible for the meter to use multiple ports at the same time. One item to not is that both Ethernet ports are the same IP and cannot be isolated networks. If you connect 2 different networks the meter will bridge them. Note that meter supports multiple Port connections on 1 Ethernet connection.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.