Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2024-08-0605:06 AM
PM8240 Communication Capabilities
Hi Team
Please may I ask you to verify if it is possible to simultaneously use the 2 x Ethernet Ports with IEC61850 and also the RS485 Port with Modbus RTU (ie can customer use all three ports simultaneously from different Masters)? for PM8240.
Yes it is possible for the meter to use multiple ports at the same time. One item to not is that both Ethernet ports are the same IP and cannot be isolated networks. If you connect 2 different networks the meter will bridge them. Note that meter supports multiple Port connections on 1 Ethernet connection.
Yes it is possible for the meter to use multiple ports at the same time. One item to not is that both Ethernet ports are the same IP and cannot be isolated networks. If you connect 2 different networks the meter will bridge them. Note that meter supports multiple Port connections on 1 Ethernet connection.