Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000 Phase order settings

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8000 Phase order settings
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Koen_Rowies
Koen_Rowies Troubleshooter
Troubleshooter

Posted: ‎2018-07-05 02:23 AM

0 Likes
5
3065
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
‎2018-07-05 02:23 AM

PM8000 Phase order settings

Hello,

At a customer site i have 2 PM8000 devices with the phasor diagram showing an ACB rotation

When Changing the parameter via the Web interface from ABC to ACB this has no influence on the phasor diagram, shouldn’t this change then to the ABC rotation?

Second question, what happens when this parameter is not correctly set? errors in PME?

Can this parameter also be set in IONsetup? I can't find it there...

Br,

Koen

Tags (2)
  • Tags:
  • phase order
  • pm8000
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 5
Bojan
Bojan Leader
Leader

Posted: ‎2018-07-05 04:41 AM

0 Likes
0
3016
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
‎2018-07-05 04:41 AM

Hi Koen,

I think that Phase Order parameter is suppose to be used in Phase Reversal Unary Alarm detection, but it's not used in PM8000 like in PM5000:

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2018-07-10 03:47 PM

0 Likes
0
3016
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
‎2018-07-10 03:47 PM

The standard ION Setup Assistant does not expose all available registers to most users (in this case, this is a wiring issue which should of been caught during meter installation).  You can view the setup registers by switching into Advanced ION Setup view (Device Properties -> Tools -> Show Advanced Setup) and going into the Power Meter modules and modifying the appropriate setup register.

While you could start swapping polarity registers, we don't recommend this as showing "software" fixed phasors may create safety concerns when servicing the device at a later time.  Another option is you can alter the phasor rotation in ION Setup but this is a global setting which affects all phasor viewers for every device that ION Setup communicates with (Tools -> Options -> Conventions).

Reply
Bojan
Bojan Leader
Leader

Posted: ‎2018-07-11 07:33 AM

0 Likes
2
3016
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
‎2018-07-11 07:33 AM

Hi Koen,

Just a remark that phasing is not standardized across Distribution Systems. For three phase generation, the phase sequence and the direction of rotation must be coordinated with a local  Distribution System.

So, If you see ACB, it doesn't mean that it is a wrong phase rotation.

Best regards,

Bojan

Reply
Koen_Rowies
Koen_Rowies Troubleshooter
Troubleshooter

Posted: ‎2018-07-11 07:49 AM

0 Likes
1
3016
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
‎2018-07-11 07:49 AM

Hello Bojan,

Indeed this is not always in our hands, the meter is correct wired in the cabinet phase 1, 2, 3 but rotation is different sometimes. I was wondering if the phase rotation parameter has some influence on the alarms in PME. i have changed them but i don't see any difference on alarms...  If it is there it should have some reason...

Br,

Koen

Reply
Bojan
Bojan Leader
Leader

Posted: ‎2018-07-11 08:15 AM

0 Likes
0
3016
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
‎2018-07-11 08:15 AM

Hi Koen,

It would trigger Phase Rotation alarm in PM5000 meter if enabled, but I'm not sure for PME.

PME has configurable Alarms, but the phase rotationerror event has to be triggered by the meter, and I think PM8000 has no such alarm.

Br,

Bojan
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.