Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84265members
353371posts

PM8000 & IEC61850

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa101813_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
6
736

PM8000 & IEC61850

Hello,

Our customer wants to bring the data of the meter connected with the seral port of PM8000 using IEC61850.

Is it possible?

Best Regards,


Accepted Solutions
sesa50168
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
648

Re: PM8000 & IEC61850

Hi Jeong-Je -

I misunderstood your original request.  I've not tried to do it, but there is the option to provide a limited number of custom quantities via IEC 61850, so you could map the readings from the serial connected devices to the custom mapping.  You may have to map the data into the meter and then map it into the 61850 modules. Of course, depending on the number of devices and amount of data, it may be easier to use a G3200 gateway, that's designed for this application.

See Answer In Context

6 Replies 6
sesa50168
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: PM8000 & IEC61850

Hi Jeong-Je -

IEC 61850 is an Ethernet based protocol, therefore it requires an Ethernet connection.  It will not not work on a serial connection.

sesa101813_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
4
648

Re: PM8000 & IEC61850

Hi John,

Thank you for your prompt reply.

I know it's an ethernet based protocol.

But in my thought if we link the data from the meters connected to serail port in PM8000 to 61850 module input in Desnger,

we could transfer the data using 61850 protocol.

Is it impossible? 

Yut
Captain
Captain
0 Likes
3
648

Re: PM8000 & IEC61850

Do you mean getting data from downstream device then link them into MMXU or MMTR module ?

sesa101813_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
2
648

Re: PM8000 & IEC61850

Hi Yut,

Yes right,

If we do that, could we make PM8000 the converter from Modbus RTU to IEC61850?

sesa50168
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
649

Re: PM8000 & IEC61850

Hi Jeong-Je -

I misunderstood your original request.  I've not tried to do it, but there is the option to provide a limited number of custom quantities via IEC 61850, so you could map the readings from the serial connected devices to the custom mapping.  You may have to map the data into the meter and then map it into the 61850 modules. Of course, depending on the number of devices and amount of data, it may be easier to use a G3200 gateway, that's designed for this application.

sesa101813_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: PM8000 & IEC61850

Hi John

Thank you fo your help.

I'm happy to know that.

Actually I considered using G3200 before but our sales guy said to me that using PM8000 in this applicatoin will be better opportunity.

Thank you John !!

Thank you Yut !!