• About sesa101813_brid
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
sesa101813_brid
sesa101813_brid
Schneider Alumni (Retired)
‎2018-09-13
61
Posts
7
Likes Received
6
Likes Given
0
Solutions

Community Badges

Open Hailing Frequencies - L4
Resistance is Futile - L4
Open Hailing Frequencies - L3
Resistance is Futile - L3
+6
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
sesa101813_brid
sesa101813_brid /html/rank_icons/Retired-User.png

Power Meter with IP44 or IP54

Hello Everyone,Do we have Power Meter with the protection level of IP44 or IP54 besides PM8000?The price for PM8000 is much higher than that of the co...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
715 0 0

2017-11-24 02:01 AM

sesa101813_brid
sesa101813_brid /html/rank_icons/Retired-User.png

Bringing in data with Automation Server into Com'X510

Hello everyone,I'd like to bring in data with Automation Server into Com'X510.In other words,Different kinds of meters with BACNet, Lonwork protocol i...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
726 0 1

2017-10-25 07:01 PM

sesa101813_brid
sesa101813_brid /html/rank_icons/Retired-User.png

Can we change the default telnet port number in ION meters?

Hi Everyone,Our customer is using ION8400,8600, 8650.They are asking whether the default telnet port number can be changed to another number for their...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1704 0 2

2017-04-02 10:05 PM

sesa101813_brid
sesa101813_brid /html/rank_icons/Retired-User.png

How to upload energy data to database system

Hi everyone,Our customer wants to bring energy data into their own database system.If they have our software such as PME, PSE, there is no problem but...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
767 0 0

2016-11-09 08:47 PM

sesa101813_brid
sesa101813_brid /html/rank_icons/Retired-User.png

Configuring RCB function for PM8000

Hi Everyone,Our customer is configuring IEC61850 function for PM8000.They want to use RCB function for the protocol between system(client) and the met...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1607 0 4

2016-09-20 06:25 PM

sesa101813_brid
sesa101813_brid /html/rank_icons/Retired-User.png

PM8000 & IEC61850

Hello,Our customer wants to bring the data of the meter connected with the seral port of PM8000 using IEC61850.Is it possible?Best Regards,
EcoStruxure Power & Grid icon_circle Metering & Power Quality
3023 0 6

2016-03-30 07:19 PM

sesa101813_brid
sesa101813_brid /html/rank_icons/Retired-User.png

About how to scale voltage value in BCPM

Hello,We're performing EMIS project with PME4DC, BCPM for Data Center.We're getting the valtage value through BCPM but the voltage line is connected t...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
650 0 0

2014-02-20 07:41 PM

Activity Feed
  • Posted Power Meter with IP44 or IP54 on Metering & Power Quality. ‎2017-11-24 02:01 AM
  • Posted Bringing in data with Automation Server into Com'X510 on Gateways and Energy Servers. ‎2017-10-25 07:01 PM
  • Got a Like for Re: Link150 Ethernet Interlinks. ‎2017-08-02 06:29 AM
  • Posted Re: Link150 Ethernet Interlinks on Metering & Power Quality. ‎2017-05-15 06:59 PM
  • Posted Re: Can we change the default telnet port number in ION meters? on Metering & Power Quality. ‎2017-04-03 06:23 PM
  • Posted Can we change the default telnet port number in ION meters? on Metering & Power Quality. ‎2017-04-02 10:05 PM
  • Posted How to upload energy data to database system on Metering & Power Quality. ‎2016-11-09 08:47 PM
  • Posted Re: Configuring RCB function for PM8000 on Metering & Power Quality. ‎2016-09-25 09:57 PM
  • Posted Configuring RCB function for PM8000 on Metering & Power Quality. ‎2016-09-20 06:25 PM
  • Got a Like for Re: PM8000 & IEC61850. ‎2016-04-04 11:28 PM
  • Got a Like for Re: PM8000 & IEC61850. ‎2016-03-31 09:01 PM
  • Posted Re: PM8000 & IEC61850 on Metering & Power Quality. ‎2016-03-31 05:17 PM
  • Posted Re: PM8000 & IEC61850 on Metering & Power Quality. ‎2016-03-31 01:55 AM
  • Posted Re: PM8000 & IEC61850 on Metering & Power Quality. ‎2016-03-30 09:32 PM
  • Posted PM8000 & IEC61850 on Metering & Power Quality. ‎2016-03-30 07:19 PM
  • Posted About how to scale voltage value in BCPM on Metering & Power Quality. ‎2014-02-20 07:41 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.