Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84255members
353353posts

PM8000 - Extended Waveform Capture

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Nicholas_Brown
Ensign Ensign
Ensign
0 Likes
6
1362

PM8000 - Extended Waveform Capture

In the PM8000 user manual, there is a reference to the meter having "Extended Waveform Capture" capability.  Looking at the Waveform Recorder Modules in Designer, I do not see the settings necessary to configure this.  Is this a mistake in the literature or perhaps it was implemented in a later FW version?

 

Link to source:

https://www.productinfo.schneider-electric.com/pm8000/594169a446e0fb0001570843/PM8000%20user%20manua...

 

 

Tags (1)

Accepted Solutions
DanL
Commander Commander
Commander

Re: PM8000 - Extended Waveform Capture

The "pre-trigger" and "post-trigger" features were part of the v2.1.0 release

https://download.schneider-electric.com/files?p_Doc_Ref=7EN12-0316

 

The latest released PM8000 firmware is now v3.0.0.

 

If you have firmware prior to v2.1, first follow these steps:
https://download.schneider-electric.com/files?p_enDocType=Firmware&p_File_Name=7EN72-0203-00_Upgradi...

 

Then follow these steps to upgrade to v3

https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=UpgradeMeterFirmwar...

See Answer In Context

Tags (1)
6 Replies 6
Tom_Stevenson
Picard Picard
Picard

Re: PM8000 - Extended Waveform Capture

Hi Nicolas

 

A few notes to hopefully help.  First - assuming you have a firmware version > 2.0.0 on the PM8000.  

 

Second, the implementation is the same across PM8000/ION7400/ION9000 etc, so you can find some ION9000 hits on this forum if you search for extended waveform like this: https://community.exchange.se.com/t5/Metering-Power-Quality/ION9000-Waveform-capture/m-p/153434

 

ION Setup also makes this a little simpler too with the wizard if that's an option for you, but you can do it from first principles in Designer for sure.

 

Hope this helps !

 

Tom

Tags (1)
DanL
Commander Commander
Commander

Re: PM8000 - Extended Waveform Capture

The "pre-trigger" and "post-trigger" features were part of the v2.1.0 release

https://download.schneider-electric.com/files?p_Doc_Ref=7EN12-0316

 

The latest released PM8000 firmware is now v3.0.0.

 

If you have firmware prior to v2.1, first follow these steps:
https://download.schneider-electric.com/files?p_enDocType=Firmware&p_File_Name=7EN72-0203-00_Upgradi...

 

Then follow these steps to upgrade to v3

https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=UpgradeMeterFirmwar...

Tags (1)
Nicholas_Brown
Ensign Ensign
Ensign
0
1356

Re: PM8000 - Extended Waveform Capture

This must be it, I'm running the simulator with v1.4.3... I'll update and check again, thanks for the help.

Tags (1)
Nicholas_Brown
Ensign Ensign
Ensign
0 Likes
2
1355

Re: PM8000 - Extended Waveform Capture

Thanks for the help.... does the ION Setup Wizard actually allow for the configuration of this... I was under the impression it did not and you had to use Designer.

Tags (1)
Charles_Murison
Picard Picard
Picard

Re: PM8000 - Extended Waveform Capture

Hello @Nicholas_Brown ,

 

Anything you can do in Designer you can do in ION Setup, Somethings are easy to do with the Setup Assistant, other things require using the Advanced configuration. 2 Differences, a) ION Setup is free, b) User interface is different.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
Nicholas_Brown
Ensign Ensign
Ensign
0 Likes
0
1331

Re: PM8000 - Extended Waveform Capture

Thanks Charles, yeah I completely disregarded the abililty to configure individual modules in ION Setup, thanks for the reminder.

Tags (1)