Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354358posts

PM5561 NTP support FW V10.1.0.0

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Koen_Rowies
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
2
643

PM5561 NTP support FW V10.1.0.0

Hello,

 

I have a customer asking how to set the NTP server on a PM5561. He can't find the settings.

I think this feature was not supported in the version 10.1.0.0 (2014). 

Firmware update is not possible on this version (MID limitations)

Could someone confirm this?

 

Br,

 

Koenpm5561.jpg


Accepted Solutions
Ramasamy_N
Commander Commander
Commander

Re: PM5561 NTP support FW V10.1.0.0

Hi Koen, 

 

Yes, PM5561 v10.1.0 does not support the NTP. 

 

You can sync the time using Modbus write function like PME or ION setup. 

 

Regards, 

Ramasamy N

See Answer In Context

Tags (1)
2 Replies 2
Charles_Murison
Picard Picard
Picard
0 Likes
0
577

Re: PM5561 NTP support FW V10.1.0.0

@Ramasamy_N  can you confirm when PM5560 supported NTP (OS version) , and if possible to configure via web.

 

Thank you,

Charles

 

L4 Prime for Advanced metering and Utilities
Tags (1)
Ramasamy_N
Commander Commander
Commander

Re: PM5561 NTP support FW V10.1.0.0

Hi Koen, 

 

Yes, PM5561 v10.1.0 does not support the NTP. 

 

You can sync the time using Modbus write function like PME or ION setup. 

 

Regards, 

Ramasamy N

Tags (1)