Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM5560 following Firmware update webpage can't be reached

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM5560 following Firmware update webpage can't be reached
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
BretNufer
BretNufer
Explorer

Posted: ‎2024-08-23 01:37 PM

0 Likes
2
1863
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
‎2024-08-23 01:37 PM

PM5560 following Firmware update webpage can't be reached

I've purchased 29 PM5560 meters to update from PM800's 

Installed 23 so far, connected 9 to network so far.

of those 9, 3 were at FW 2.8.3, the other 6 were at 4.1.8

different webpage structure, security, etc. so I thought I would update them to match.

I installed the PM5000 Firmware update tool V3.10 it came with FW V4.2.1, I decided to bring everything up to 4.2.1

So that's the background, here's the problem...

The three that updated from 2.8.3, two of them went through the update 'fine' and I was able to get on the website and enter the MAC address as the password and immediately updated the password, the 3rd did not. 

Now none of those three allow web access, the web browser returns "ERR_CONNECTION_REFUSED" 

the Firmware update tool Shows that the two of the three that updated the password are at the new FW level

the all three show updated from the screen on the devices.  Tried cycling power, enabling/disabling FTP, etc. Cannot disable HTTP from the keypad

I get a good Ping return, and the other meters are working fine. tried a direct cable from laptop to meter, tried a second laptop, swapped between the two ports on the meter, etc.  I've tried everything I can think of.

 

Appreciate any suggestions

Labels
  • Labels:
  • PM5000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Jesus_Diaz
Jesus_Diaz Leader
Leader

Posted: ‎2024-09-19 11:20 AM

1 Like
1
1793
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
‎2024-09-19 11:20 AM

Hello @BretNufer ,

 

In FW 4.1.3 and later, HTTP was replaced with HTTPS. Please make sure that you are using "https" in the web browser address bar, for example, "https://xxx.xxx.xxx.xxx/".

 

Also, make sure that the HTTPS server is enabled in the meter using the front panel:

 

Jesus_Diaz_0-1726769988953.png

 

Best Regards,

JD

 

See Answer In Context

Reply
Replies 2
Jesus_Diaz
Jesus_Diaz Leader
Leader

Posted: ‎2024-09-19 11:20 AM

1 Like
1
1793
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
‎2024-09-19 11:20 AM

Hello @BretNufer ,

 

In FW 4.1.3 and later, HTTP was replaced with HTTPS. Please make sure that you are using "https" in the web browser address bar, for example, "https://xxx.xxx.xxx.xxx/".

 

Also, make sure that the HTTPS server is enabled in the meter using the front panel:

 

Jesus_Diaz_0-1726769988953.png

 

Best Regards,

JD

 

Reply
BretNufer
BretNufer
Explorer

Posted: ‎2024-09-20 05:27 AM

0 Likes
0
1767
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
‎2024-09-20 05:27 AM

HTTPS has been enabled all along, couldn't disable it from the display.

 

I'm not sure exactly what action or combination of actions resolved this, but it did start responding again and is resolved.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.