Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM5560 Rogue DHCP IP Address

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM5560 Rogue DHCP IP Address
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
solutions_iems-
solutions_iems-
Troubleshooter

Posted: ‎2025-05-23 02:17 AM

0 Likes
1
985
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
‎2025-05-23 02:17 AM

PM5560 Rogue DHCP IP Address

I have recently installed 12 no. PM5560 power meters on a site and connected all to the site LAN configured for DHCP.

 

Of the 12 no. power meters, 10 no. have connected and picked up an IP address from the site DHCP server in the range 150.237.194.xxx, but 2 no. power meters have "rogue" IP addresses of 85.16.192.217 and 85.16.199.249

 

My client insists that these IP addresses are not being supplied by their DHCP server but relate to two different locations in Germany! How can this be when the power meters are installed in the UK!

 

Any feedback will be appreciated.

 

Thank you.

Labels
  • Labels:
  • PM5000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-05-23 04:32 AM

0 Likes
0
966
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
‎2025-05-23 04:32 AM

Hi @solutions_iems- 

 

As mentioned in PM5500 user guide, the 85.16.xxx.xxx is the default first two values of the IP address in Acquisition Mode, and the last two values of the IP address are the last two hexadecimal values of the MAC address converted to decimal: 

Mehran_Mehrnia_0-1747999433932.png

 

As for the two meters that have not obtained an IP address from the DHCP server, further investigation is required into the device network configuration, such as verifying whether DHCP is enabled, no static IP is set, and ensuring proper cable and network connections, etc.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Reply 1
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-05-23 04:32 AM

0 Likes
0
966
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
‎2025-05-23 04:32 AM

Hi @solutions_iems- 

 

As mentioned in PM5500 user guide, the 85.16.xxx.xxx is the default first two values of the IP address in Acquisition Mode, and the last two values of the IP address are the last two hexadecimal values of the MAC address converted to decimal: 

Mehran_Mehrnia_0-1747999433932.png

 

As for the two meters that have not obtained an IP address from the DHCP server, further investigation is required into the device network configuration, such as verifying whether DHCP is enabled, no static IP is set, and ensuring proper cable and network connections, etc.

 

Best Regards,

-Mehran

L3 Expert Advanced metering
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.