Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
So I am having issues getting the command semaphore through modbus using a red lion gateway with controllogix PLC.
I plan to get/read the command semaphore from Modbus register 405680 and then write that number to Modbus register 405001 and write 2020 to Modbus register 405000. So far I am unable to get that command semaphore from the red lion gateway.
I'm trying to reset all energies automatically every month. Is there another suggestion on how I can accomplish that?
Link copied. Please paste this link to share this article on your social media post.
Hi @Jemeu,
The "reset all energy" command can be used in the unprotected command interface (without semaphore; you can just use a value of 0).
Please find an example using Modbus Tester and how it looks in Wireshark:
Thank you,
JD
Link copied. Please paste this link to share this article on your social media post.
Hi @Jemeu,
The "reset all energy" command can be used in the unprotected command interface (without semaphore; you can just use a value of 0).
Please find an example using Modbus Tester and how it looks in Wireshark:
Thank you,
JD
Link copied. Please paste this link to share this article on your social media post.
Thank you very much for your help. I'm using an Allen-Bradley Control Logix PLC with a Red Lion Gateway to send Modbus commands.
This worked with the Generic Modbus tester, however I was having trouble resetting the energy monitor with the PLC.
For some reason, it only works if I write 2020 in 405250 and 1 in 405251. Not a big problem though it works as it should now.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.