New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Missing template feature set information error
Metering & Power Quality
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
2017-03-1309:22 PM
Missing template feature set information error
"missing template feature set information" error popups up when upgrading a PM8k meter using ion setup build 17069. Upgrade seems to work but the error popups up before beginning the download of the dcf to the meter, it also takes a very long time (30mins) before eventually the upgrade fails but the meter seems to function and firmware shows upgraded. !
Link copied. Please paste this link to share this article on your social media post.
2017-03-3001:51 PM
This is a known issue that was resolved with the next available build (3.0.17073.1) as there was a bug in older versions which were not properly recording the feature set information into appropriate DCF files.
While adding this dialog reporting the issue, it should of been restricted to only models which actually has a feature set code (which the PM8000 does not) so this was fixed in the next released build.
Subsequently if you do see this error, you should download the template, then save a new DCF file *IF* you are doing so for a model with feature set information (such as an ION8650A for example).