Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Map a modbus register to a digital input on ION7650

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Map a modbus register to a digital input on ION7650
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
sesa389533_brid
sesa389533_brid Leader
Leader

Posted: ‎2017-12-15 01:42 AM . Last Modified: ‎2020-04-22 01:14 AM

0 Likes
1
1128
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
‎2017-12-15 01:42 AM

Map a modbus register to a digital input on ION7650


Hello,

 

Is it possible to map a modbus register to a digital input ?

 

Thanks

 

François

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-12-22 08:12 PM

0 Likes
0
1091
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
‎2017-12-22 08:12 PM

I am assuming you are asking if it is possible to map the detected input status of one of the ION7650's digital inputs into an available Modbus register that can be read via Modbus?

If so, the answer is yes.  This can be done via the Advanced ION view (or alternatively using ION Designer in PME).  You would need to connect the one of the Digital Input modules output (one of which you have correctly assigned the port setup register to the desired hardware port) and feed that output into an input of a  newly created Convert module (this is to alter the Boolean output of the digital input to a numeric value (0 or 1).  Subsequently you would then connect the Convert output to the input of one of the Modbus Slave modules (or create a new one if available) and assign an appropriate starting register and register format.

You should then be able to use a Modbus master and poll that register and should return a value of 0 or 1 indicating the status of the digital input.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.