Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Is there any IEEE 519:2014 framework compatible with ION8650A available?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Is there any IEEE 519:2014 framework compatible with ION8650A available?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
Ramasamy_N
Ramasamy_N Champion
117
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
PowerLogic
PowerLogic ION8650 series
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
Sreejith_KM
Sreejith_KM Contributor
Contributor

Posted: ‎2023-02-01 11:49 AM

0 Likes
8
4637
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
‎2023-02-01 11:49 AM

Is there any IEEE 519:2014 framework compatible with ION8650A available?

Hi

We have a requirement where we need to show IEEE 519:2014 compliance report using PME and ION8650A.

Understand it is not default available in the meter. Do we have any framework compatible with ION8650A available? Or can we use the framework for ION9K in ION8650A?

  • Thumbnail of PowerLogic ION8650 series
    PowerLogic
    PowerLogic ION8650 series
View products (1)
Labels
  • Labels:
  • ION Guidebooks
  • ION8000
  • Power Quality
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
N4th4n13L
N4th4n13L Troubleshooter
Troubleshooter

Posted: ‎2023-02-02 07:11 PM

2 Likes
1
4609
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
‎2023-02-02 07:11 PM

Hello @Sreejith_KM ,

 

I created the attached framelet when working on this for the US template. I would only recommend pushing this with PME Designer as it will likely overwrite several modules in the existing framework. I know I had to remove most the EN50160 recorders for this to fit. I was using the US template so it also utilizes the floating nominal framework for nominal voltage. It also uses some overlapping modules with the 4-30 framework, and may create duplicate modules when pushing. I remember the label names need to be correct feeding the data recorders for the PME report to run as well. I used a 9000 meter to reference the label names to make sure they're correct. 

See Answer In Context

Attachments
8650A_IEEE519_V3.zip
Reply
Replies 8
N4th4n13L
N4th4n13L Troubleshooter
Troubleshooter

Posted: ‎2023-02-01 02:53 PM

2 Likes
7
4627
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
‎2023-02-01 02:53 PM

Hello,

 

The US V4.2.0.2.2 template does include the framework in it. It's built based on the ION 9000 framework, but had to allocate modules a little differently based on core framework already in the US template.

Reply
Sreejith_KM
Sreejith_KM Contributor
Contributor

Posted: ‎2023-02-01 09:56 PM

0 Likes
4
4621
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
‎2023-02-01 09:56 PM

Thanks for the reply.

So, guess for India with FW V4.40.1, we don't have any option than making a new custom framework.

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-02-02 10:12 AM

1 Like
3
4615
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
‎2023-02-02 10:12 AM

Hello @Sreejith_KM , have you talked with Pradip Maity? I believe there is currently a piolet running in India with ION8650 meters and US V4.2.0.2.2 template.


Regarding a custom framework, if you want to create your own you are welcome to do so, there is nothing saying you cannot. Note that the IEE519 is a complex framework with many modules and PME is very specific as to what needs to be recorded for the report to work.

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
N4th4n13L
N4th4n13L Troubleshooter
Troubleshooter

Posted: ‎2023-02-02 07:11 PM

2 Likes
1
4609
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
‎2023-02-02 07:11 PM

Hello @Sreejith_KM ,

 

I created the attached framelet when working on this for the US template. I would only recommend pushing this with PME Designer as it will likely overwrite several modules in the existing framework. I know I had to remove most the EN50160 recorders for this to fit. I was using the US template so it also utilizes the floating nominal framework for nominal voltage. It also uses some overlapping modules with the 4-30 framework, and may create duplicate modules when pushing. I remember the label names need to be correct feeding the data recorders for the PME report to run as well. I used a 9000 meter to reference the label names to make sure they're correct. 

Attachments
8650A_IEEE519_V3.zip
Reply
Sreejith_KM
Sreejith_KM Contributor
Contributor

Posted: ‎2023-02-03 12:54 AM

0 Likes
0
4601
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
‎2023-02-03 12:54 AM

Thanks very much @Charles_Murison for the response.

Lately came to know about this project and now connected with Pradip.

Reply
Sreejith_KM
Sreejith_KM Contributor
Contributor

Posted: ‎2023-02-03 01:01 AM

0 Likes
0
4600
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
‎2023-02-03 01:01 AM

Thanks very much @N4th4n13L, appreciate your help in this regard.

Will update the shared info to backend team to adapt & see.

Reply
LarryP
LarryP
Explorer

Posted: ‎2024-11-21 11:35 AM

0 Likes
1
3231
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
‎2024-11-21 11:35 AM

For the 8650A voltage range setting.  Is the below correct?; i.e. the radio buttons L-L while the nominal is L-N?

LarryP_0-1732217631802.png

 

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-11-22 09:00 AM

0 Likes
0
3217
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
‎2024-11-22 09:00 AM

Hello @LarryP ,

 

Will need to refer to the IEEE519 Standard to confirm if the voltage is VLL or VLN. As far as the meter is concerned, this setting will change an External Numeric register that has enumeration for PME reports. This setting will also affect the table ION Setup uses to program the harmonic limits. This does not affect the sag/swell module.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.