Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Is there ModBus access and Mapping for PowerLogic PM5563 ?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Is there ModBus access and Mapping for PowerLogic PM5563 ?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
Schneider Electric
PowerLogic PM5000 series

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
NortheastSolar
NortheastSolar
Explorer

Posted: ‎2025-02-28 06:47 PM

0 Likes
6
3177
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
‎2025-02-28 06:47 PM

Is there ModBus access and Mapping for PowerLogic PM5563 ?

I need to automate the download of all our meter data on a daily basis. 

 

Does PowerLogic PM5563 have TCP/IP modbus access through the ethernet port?

 

If so, is there a published access guide and modbus map you can point me to?

 

If not, what is the most direct way to automate the download of logs?

 

Thanks

  • Thumbnail of PowerLogic PM5000 series
    Schneider Electric
    PowerLogic PM5000 series
View products (1)
Labels
  • Labels:
  • PM5000
Tags (5)
  • Tags:
  • automation
  • Data Log
  • english
  • metering
  • modbus
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-03-03 08:56 AM

1 Like
1
3160
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
‎2025-03-03 08:56 AM

Hi @NortheastSolar 

 

Yes, the PM5500, such as the PM5563, has an Ethernet port that allows data to be polled via port 502 through Modbus. The Modbus map can be found in the device firmware package, which can be downloaded from the 'Software and Firmware' section on the Schneider Electric website. 

 

Meter also has the 'Log Export' feature (has been enabled again in fw V4.4.5) to export its logs to a web server, either on a schedule or manually.

For more information, please refer to the section 'Setting Up Device Log Exports Using the Webpages' in the PM5500 user guide on page 132.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Replies 6
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-03-03 08:56 AM

1 Like
1
3161
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
‎2025-03-03 08:56 AM

Hi @NortheastSolar 

 

Yes, the PM5500, such as the PM5563, has an Ethernet port that allows data to be polled via port 502 through Modbus. The Modbus map can be found in the device firmware package, which can be downloaded from the 'Software and Firmware' section on the Schneider Electric website. 

 

Meter also has the 'Log Export' feature (has been enabled again in fw V4.4.5) to export its logs to a web server, either on a schedule or manually.

For more information, please refer to the section 'Setting Up Device Log Exports Using the Webpages' in the PM5500 user guide on page 132.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
NortheastSolar
NortheastSolar
Explorer

Posted: ‎2025-03-03 01:48 PM

0 Likes
0
3136
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
‎2025-03-03 01:48 PM

Oh wow, Mehran thanks so much

 

Please be advised, the detachable display version of this meter does not have updated firmware information:

https://www.se.com/us/en/product/METSEPM5563RD/power-meter-powerlogic-pm5563-2-ethernet-up-to-63th-h...

 

Can I assume the firmware is compatible, or no? 

 

NortheastSolar_0-1741038188783.png

 

Reply
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-03-04 09:43 AM . Last Modified: ‎2025-03-04 02:46 PM

1 Like
1
3122
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
‎2025-03-04 09:43 AM

Hi @NortheastSolar 

 

You're welcome.

 

In the website, the released firmware V4.4.5 is referring to both PM5560 and PM5563 without remote display:

Mehran_Mehrnia_0-1741109571302.png

 

Sine both offers PM5563 and PM5563 with remote display have the same meter, you can upgrade them with V4.4.5 and likely the website needs to be updated for latest firmware of PM5563 with remote display.

 

Hi @Ramasamy_N please advise.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
NortheastSolar
NortheastSolar
Explorer

Posted: ‎2025-03-04 11:10 AM

1 Like
0
3108
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
‎2025-03-04 11:10 AM

Thanks again, I can confirm that the new firmware V4.4.5 firmware upgrade worked for the PM5563 meter with detachable display.

 

A note for anyone struggling with the password requirement - once upgraded to V4 firmware a new user is created with username "Administrator" and password corresponding to the uppercase MAC address with no dashes.

 

If you are not on site and only have the IP of the meter, in windows open a command prompt and ping the meter address (ie 10.0.0.52), followed by "arp -a 10.0.0.52" which would give you a MAC address like 00-80-67-89-56-aa 

 

The meter password would then be  "0080678956AA"

Reply
NortheastSolar
NortheastSolar
Explorer

Posted: ‎2025-03-10 11:56 AM

0 Likes
0
3051
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
‎2025-03-10 11:56 AM

So we've hit a snag, the Data Log Export feature in this firmware version does not allow us to specify the target path of the data post, that value is greyed out. We cannot get the data posting to work with this forced value

 

Is there a work around to changing the path from "/api/datalog/httptest" to the web page where we receive data like in firmware version  2.7.4   ?

 

Is there documentation for this updated posting feature?

Reply
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2025-03-28 08:28 AM

0 Likes
0
2953
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
‎2025-03-28 08:28 AM

Hello @NortheastSolar 

 

The logs will be export to the fixed path (uploads folder) for in the firmware v4.4.5, there is no option to change this path.

 

Regards, 

Ramasamy N
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.