Hello SE support,
I am using ION8650 offline meter to do dynamic programming, have questions:
1. where can I download the V4.40 offline ION8650 simulator?
2. I have one ION8650 connected locally to my laptop as a Modbus master, is there a way to connect one or multiple offline ION meters as Modbus slave?
Thanks
Leo
- Labels:
-
ION8000
Accepted Solutions
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
Hello @Liangchen1982 ,
1) There is no public V4.40 offline ION8650 simulator?
2) No, not possible to setup the ION8650 offline simulator as a modbus slave.
Regards,
Charles
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
Hello @Liangchen1982 ,
1) There is no public V4.40 offline ION8650 simulator?
2) No, not possible to setup the ION8650 offline simulator as a modbus slave.
Regards,
Charles