Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION8650 integrated using IEC-61850, cVal.mag values are in Bad quality and without time stamp

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION8650 integrated using IEC-61850, cVal.mag values are in Bad quality and without time stamp
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Pepz
Pepz
Contributor

Posted: ‎2025-08-15 03:14 PM

0 Likes
6
1976
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
‎2025-08-15 03:14 PM

ION8650 integrated using IEC-61850, cVal.mag values are in Bad quality and without time stamp

I am integrating ION8650C Power meters to 800xA System DCS using IEC-61850 protocol, I can read almost all the data, but I have problems with all data ending in "cVal.mag" (currents, voltages), becasue when the values of this data change, the changes are automatically displayed but with Bad quality and without time stamp.

Power meter model: M8650C7C0H6E1A0A

File used: SE_ION_8650-C-F01_E2V01.icd

I attached screenshots.

Pepz_0-1755295963071.png

 

 

 

 

Attachments
Screenshots.7z
Labels
  • Labels:
  • ION8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Pepz
Pepz
Contributor

Posted: ‎2025-08-27 03:46 PM

0 Likes
1
1869
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
‎2025-08-27 03:46 PM

Hi Mehran,

 

I have used the default values for the RCB parameters, which are the same as those are you suggest.

Pepz_0-1756334383448.png

 

It seems that the problem is on the 800xA system side, I have requested assistance.

I will let you know if I manage to solve it.

 

Thank you

See Answer In Context

Reply
Replies 6
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-08-18 11:59 AM . Last Modified: ‎2025-08-18 12:15 PM

1 Like
4
1967
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
‎2025-08-18 11:59 AM

Hi @Pepz 

 

Please make sure the dataset includes the Data Attribute Level e.g., cVal.mag, q, t and not just Data Object Level e.g., PhV, A, PPV.

 

In IEC 61850:

Logical Node: e.g., MMXU1
Data Object: e.g., PhV, A, PPV
Data Attribute: e.g., cVal.mag, q, t


If your dataset only includes the Data Object (like PhV or A) without specifying the Data Attribute (like cVal.mag, q and t), the client may not receive the actual measurement values, timestamps, or quality indicators.


You can also use some IED Explorer or IEDScout Tools to confirm whether the issue is with the meter or the 800xA client.

Mehran_Mehrnia_0-1755543646752.png

 

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Pepz
Pepz
Contributor

Posted: ‎2025-08-26 10:04 AM

0 Likes
3
1891
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
‎2025-08-26 10:04 AM

Hi Mehran,

 

Thanks for your response.

Initially, I used the total Datasets and RCBs generated for default, without changing anything on the map. The result was that I obtained values that changed automatically but with Bad quality and no timestamp. This only happens with data with values per phase (currents, voltages,...). If I update manually (polling) I can read perfectly: good values, good quality and timestamp, the problem is the automatic update.

Now, I have tried modifying the "MMXU" Dataset to include the Data Attribute Level, but this time I can't see any values. 

In both situations I can see the values with IEC Explorer, with good quality and timestamp. 

I would appreciate it if you could show me an example of "MMXU" Dataset of an ION8650 integrated by IEC61850 from any application you have done before.

 

Pepz_0-1756227836604.png

 

Reply
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-08-27 01:03 PM . Last Modified: ‎2025-08-27 01:05 PM

0 Likes
2
1878
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
‎2025-08-27 01:03 PM

Hi @Pepz 

 

You're welcome. 

 

If manual polling retrieves correct values with good quality and timestamp but automatic updates shows bad quality and no timestamp using default datasets and RCBs, then likely it is due to how the Report Control Blocks (RCBs) and Datasets are configured in the CID file and how they are parsed in 800xA System client.

 

I usually generates the CID file using CET850 and test the result using IED Explorer. What I would suggest is, checking RCB Settings and ensure the RCB has: TrgOps with dchg=true, qchg=true, period=true,

OptFields with timeStamp=true, reasonCode=true, seqNum=true

 

CET850:

Mehran_Mehrnia_0-1756323575199.png

 

editing CID file:

Mehran_Mehrnia_1-1756323974371.png

 

IED Explorer shows correct data, therefore the dataset works in IED Explorer, client 800xA still shows bad quality and no timestamp, please verify if its IEC 61850 parser supports DA-level references.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Pepz
Pepz
Contributor

Posted: ‎2025-08-27 03:46 PM

0 Likes
1
1870
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
‎2025-08-27 03:46 PM

Hi Mehran,

 

I have used the default values for the RCB parameters, which are the same as those are you suggest.

Pepz_0-1756334383448.png

 

It seems that the problem is on the 800xA system side, I have requested assistance.

I will let you know if I manage to solve it.

 

Thank you

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-08-28 11:59 AM

0 Likes
0
1857
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
‎2025-08-28 11:59 AM

Hello @Pepz ,

If using a report subscription, the ION8650 meter does not send a timestamp attribute for each measurement, the timestamp of the report is the timestamp for all measurements in the report.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Pepz
Pepz
Contributor

Posted: ‎2025-10-10 05:09 PM

0 Likes
0
1682
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
‎2025-10-10 05:09 PM

Hi,

I would like to note that the issue was resolved by modifying the Datasets from CET850:

I have tested modifying the Datasets from CET850 to include all the Data Objects and we got quality and time stamps for the values.

Pepz_0-1760141245877.png

I appreciatte all your support. 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.