Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION8650 Dynamic programming connection limitation

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION8650 Dynamic programming connection limitation
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
Liangchen1982
Liangchen1982
Explorer

Posted: ‎2024-05-15 01:20 PM

0 Likes
1
1028
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
‎2024-05-15 01:20 PM

ION8650 Dynamic programming connection limitation

Hello SE experts,

 

The ION8650 meter supports a maximum of eight simultaneous Ethernet connections, however, I have dynamic programming site that more than 8 sub meters need to be connected to the modbus master meter. 

 

Any solution to address this issue?

 

Thanks

Leo

Labels
  • Labels:
  • ION8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2024-05-16 01:30 PM . Last Modified: ‎2024-05-16 01:34 PM

1 Like
0
1011
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
‎2024-05-16 01:30 PM

The ION8650 can support up to 10 Modbus Master TCP connections (which are completely separate from the 8 incoming connection restriction).

Robert_Lee_0-1715891338418.png

So if you have 8 separate IP addresses, this is supported presently.  If you need more, I'd recommend daisy chaining some of the devices via RS-485 and gateway a few together.


But if you are implying that there are *eight* Modbus Master which want to access the ION8650, then the only recourse would be to likely use some type of Modbus gateway (like ComX or Link150 or HEP ION meter) and connect the ION8650 serially.  The Modbus gateway will allow multiple masters to connect and alternate the requests sent to the ION8650.

See Answer In Context

Reply
Reply 1
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2024-05-16 01:30 PM . Last Modified: ‎2024-05-16 01:34 PM

1 Like
0
1011
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
‎2024-05-16 01:30 PM

The ION8650 can support up to 10 Modbus Master TCP connections (which are completely separate from the 8 incoming connection restriction).

Robert_Lee_0-1715891338418.png

So if you have 8 separate IP addresses, this is supported presently.  If you need more, I'd recommend daisy chaining some of the devices via RS-485 and gateway a few together.


But if you are implying that there are *eight* Modbus Master which want to access the ION8650, then the only recourse would be to likely use some type of Modbus gateway (like ComX or Link150 or HEP ION meter) and connect the ION8650 serially.  The Modbus gateway will allow multiple masters to connect and alternate the requests sent to the ION8650.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.