Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION7650 does not communicate with PME and IONSetup

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION7650 does not communicate with PME and IONSetup
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Ricardo_RM
Ricardo_RM
Contributor

Posted: ‎2023-05-24 07:28 AM . Last Modified: ‎2023-05-24 07:31 AM

0 Likes
7
3651
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
‎2023-05-24 07:28 AM

ION7650 does not communicate with PME and IONSetup

hello community

A few days ago an ION 7650 does not allow connecting to the PME, nor to the ION Setup.

 

As seen in the image, if there is communication on the network, then it pings.

 

Ricardo_RM_0-1684937482867.jpeg


But when you try to connect to the Magnament Console, it says that it cannot connect. Nor when entering ION Setup, where the message that appears is that it is not "unable to contact device".

 

Ricardo_RM_1-1684938223213.jpeg

 

And it has tried to enter the web server of the meter, but it still does not work. As seen in the following image

 

Ricardo_RM_2-1684938375613.jpeg

 

Any information would help me. Many thanks for everything.

@Charles_Murison 

@Attila_Fritz 

Labels
  • Labels:
  • ION Setup
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-06-02 11:13 AM

0 Likes
0
3577
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
‎2023-06-02 11:13 AM

Hello @Ricardo_RM ,

The serial port(s) of a meter can talk ION and be used to communicate with meter using ION Setup. Note that serial communications are significantly slower than Ethernet communications.

 

Depending on the firmware version of the meter, you could try using Telnet to communicate to the meter. Not much settings you could change but does help test communications.

If you remove the meter from the network does Ping still respond?


Did you try power cycle the meter?

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 7
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-05-24 09:35 AM

0 Likes
0
3642
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
‎2023-05-24 09:35 AM

Hello @Ricardo_RM ,

 

This is a loaded question and there could be a few things that could be happening. The first thing I will say is that ping is a very, very low test. What this tells me is something on the network replied to the ping broadcast. It could be a duplicate IP address on the network and what you think you are talking to is not a meter.

Could be network is blocking ports. Ports 80 (http) 7700 (ION, PME + ION Setup). Unusual to have port 80 blocked so I would test if there are possibly another devices on the network with that IP address. 

If you connect directly to the meter are you able to communicate?

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Ricardo_RM
Ricardo_RM
Contributor

Posted: ‎2023-05-24 09:41 AM

0 Likes
3
3640
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
‎2023-05-24 09:41 AM

Hello @Charles_Murison 

 

If I forgot to comment that I did the tests by connecting the meter directly to the computer and I had no results.

 

But other meters were also tested and whether they were working normally.

 

Greetings

Reply
p_dejarmy_encos
p_dejarmy_encos
Troubleshooter

Posted: ‎2023-05-24 11:10 AM

0 Likes
1
3636
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
‎2023-05-24 11:10 AM

Hello Ricardo,

 

Are you able to communicate with the meter using the serial ports?

 

Best regards,

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-05-24 12:06 PM

0 Likes
2
3635
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
‎2023-05-24 12:06 PM

If connecting to the meter directly, did you make sure your computer's IP address was in the same subnet as the meter? This is combination of IP address and subnet mask. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Ricardo_RM
Ricardo_RM
Contributor

Posted: ‎2023-06-01 12:18 PM

0 Likes
0
3588
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
‎2023-06-01 12:18 PM

Hello @p_dejarmy_encos 

 

It has not been tested, can this type of communication use the same functions as if it were connected with Ethernet?

 

Greetings.

 

 

 

Greetings.

Reply
Ricardo_RM
Ricardo_RM
Contributor

Posted: ‎2023-06-01 12:20 PM

0 Likes
1
3588
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
‎2023-06-01 12:20 PM

Hello,

 

Correct, the same subnet was put in that was in the computer and in the meter. And I tried another meter and if it worked normally when connected directly.

 

Greetings

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-06-02 11:13 AM

0 Likes
0
3577
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
‎2023-06-02 11:13 AM

Hello @Ricardo_RM ,

The serial port(s) of a meter can talk ION and be used to communicate with meter using ION Setup. Note that serial communications are significantly slower than Ethernet communications.

 

Depending on the firmware version of the meter, you could try using Telnet to communicate to the meter. Not much settings you could change but does help test communications.

If you remove the meter from the network does Ping still respond?


Did you try power cycle the meter?

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.