Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84428members
353621posts

ION7650 current probe selection

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Ken_Hsu
Commander Commander
Commander
0 Likes
1
295

ION7650 current probe selection

Hi everyone,

I have a question about CT selection with ION7650.This is a retrofit project. 380V. The load I am measuring fluctuates up to 630A.

If I select the "Current Probe Inputs" option,  which CT models are compatible? Is it the 1VAC or 0.333VAC, or both?

Also, are there technical specs and dimensions for the different model current probes? I would like to compare the current probe option to the split core 5A ct option, in terms of ease of installation, setup and accuracy.

Apologies in advance if it is written in a manual. I could not find any drawings in the ION7650 technical data sheet and the Current Probe Input Option document.

Tags (3)
1 Reply 1
Yut
Captain
Captain

Re: ION7650 current probe selection

I used many option F meters in the past project mostly use with the M1UB 10A1V.

You can download the datasheet from .Universal Technic - Accueil  (now they become Fluke).