Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION7650 Reset IP without Display

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION7650 Reset IP without Display
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa88669
sesa88669 Contributor
Contributor

Posted: ‎2017-02-21 01:36 PM

0 Likes
3
1999
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
‎2017-02-21 01:36 PM

ION7650 Reset IP without Display

I have an ION7650 without the display. I used the web interface to change the IP and now I am not sure what the IP is. I have lost all connectivity to it. How do I restore the IP to either default or get in to change it? Again, there is no display, just the base with the network card.

On another note, I used ION Setup to change the IP on another device and once I change the IP, it sent the update to the device. I wasn't able to change the Netmask or Gateway without going through the display. That is a concern.

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
Yut
Yut
Leader

Posted: ‎2017-02-21 09:08 PM

0 Likes
0
1901
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
‎2017-02-21 09:08 PM

try to use serial ports either 232 or 485.

Reply
patrickw
patrickw Contributor
Contributor

Posted: ‎2017-02-22 05:09 PM

4 Likes
1
1901
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
‎2017-02-22 05:09 PM

When the 7650 device powers up, it will send out a gratuitous ARP packet, containing its current IP address.  If you have wireshark installed and connected to the same switch as the 7650, or directly to the meter, you will be able to capture the ARP packet (which is a layer 2 broadcast packet).  You can filter based on the source MAC address of the device to simplify finding this packet. 

I believe the timing for the packet being sent is around 10-20 seconds after powerup.

Reply
michael_franz
michael_franz
Mentor

Posted: ‎2017-05-31 11:51 AM

0 Likes
0
1901
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
‎2017-05-31 11:51 AM

Wireshark I wish I knew you well.  Does work for this sometimes....
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.