Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION setup - Complete data set download from a meter

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION setup - Complete data set download from a meter
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Grant_IPACS
Grant_IPACS
Mentor

Posted: ‎2020-04-13 12:21 AM . Last Modified: ‎2020-04-22 01:00 AM

0 Likes
4
4590
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
‎2020-04-13 12:21 AM

ION setup - Complete data set download from a meter

Hi All,

 

Maybe i'm missing something, but is there a way to do a complete download / extraction of ALL log files and waveforms, etc from a single device, with only a couple of mouse clicks?

 

This seems like a pretty obvious feature for such a mature platform to be missing.

 

The only way i see this is possible today is going to each log file, and copy / paste into excel or similar.

There is a risk that someone may not click on each log file, and data is then lost forever.

 

Reason i ask is we have a client that has asked us to alter every meters logging interval, and in doing this, it prompts us all log data may be lost, and a backup is recommended.

 

There are many meters that make up this project, some from before our time on site, and we don't seem to have the config password to access some meters, and the building manager doesn't know where to start, as she has only been in the position 18 months and cant seem to find them in any obvious location.

 

So i guess its really 2 questions, with the second, how to crack passwords...

 

Thanks 

 

Grant

 

 

Regards

Grant
Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2020-04-14 12:00 PM

0 Likes
0
4578
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
‎2020-04-14 12:00 PM

The data collection wizard should attempt to collect all available log data for that *ONE* device given what available data is on the device.  It's primary purpose however is to allow you to push that data into a PME system.

ION Setup is not an automated data collection tool.  It's primarily a device configuration tool which has many various other features which we provide *FREE* of charge.


PME on the other hand is a data collection system which will automatically store device data shortly after it occurs which users have to license per device in their system.  It sounds like if the data is important to be collected, then the user should consider this route.

Also most of the non-ION devices you listed do not support any type of file-based storage mechanism using ION Setup (such as the lower end products like PM5xxx and iEM products).

See Answer In Context

Reply
Replies 4
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-04-13 03:53 PM

0 Likes
3
4585
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
‎2020-04-13 03:53 PM

Hello @Grant_IPACS

 

A little more information is needed like, what version of ION Setup you have, what meter types and firmware version.

 

For the data collection, have you looked at Setup Assistant -> Reports -> Data Collection?

This will write information into an XML file. 

 

For meter password, different story. With increased cyber security, may of the old ways of accessing a meter have long since been closed off. Even options like brute force trial and error have lockouts now. It is possible that when programming the meters, whoever did the work saved the configuration file?

 

Charles

L4 Prime for Advanced metering and Utilities
Reply
Grant_IPACS
Grant_IPACS
Mentor

Posted: ‎2020-04-14 12:38 AM

0 Likes
2
4583
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
‎2020-04-14 12:38 AM

Hi and thanks Charles,

 

latest ION setup (? V3.2)

 

i did try that data collection thing... it ran for a few hours, and i got a tiny xml file that seemed useless, maybe i did something wrong?

 

meters are 7650, 9000, 8000, 5560, 5350, iem 3255's.

 

i think the integration  was not one single integrator, possibly many over time... some have defaults,. some do not.

 

BR 

Grant

Regards

Grant
Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2020-04-14 12:00 PM

0 Likes
0
4578
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
‎2020-04-14 12:00 PM

The data collection wizard should attempt to collect all available log data for that *ONE* device given what available data is on the device.  It's primary purpose however is to allow you to push that data into a PME system.

ION Setup is not an automated data collection tool.  It's primarily a device configuration tool which has many various other features which we provide *FREE* of charge.


PME on the other hand is a data collection system which will automatically store device data shortly after it occurs which users have to license per device in their system.  It sounds like if the data is important to be collected, then the user should consider this route.

Also most of the non-ION devices you listed do not support any type of file-based storage mechanism using ION Setup (such as the lower end products like PM5xxx and iEM products).

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-04-14 01:20 PM

0 Likes
0
4577
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
‎2020-04-14 01:20 PM

Hello Grant.

 

ION Setup has a numbering system besides just V 3.2, you would see a series of numbers afterwards, like 20091. I cannot speak to the  5560, 5350, iem 3255's meters, but with the 7650, 9000, 8000, you should be able to extract the data. If you are having trouble, I recommend contacting technical support. Be sure to include a screenshot of ION Setup options, an extract of a data recorder and the .xml file generated.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.