Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION meter configuration for 3W-Wye

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION meter configuration for 3W-Wye
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
571
Mehran_Mehrnia
Mehran_Mehrnia Champion
202
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
RobGraham
RobGraham Champion
Champion

Posted: ‎2024-12-18 03:08 AM

0 Likes
2
1546
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
‎2024-12-18 03:08 AM

ION meter configuration for 3W-Wye

I am at a site where the wye transformers have been grounded through an HRG--no neutral is pulled back to the breakers or the meters.  When I arrived, the meters were configured as 3W-Wye, which seems to make sense. 

 

What caught my attention was that some meters had the nominal voltage set to the L-L nominal, and some L-N.  Those with L-L are capturing PQ events normally, while the L-L meters are not.  This seems to contradict the ION Reference:  

 

NOTE: Nominal refers to the primary power system RMS voltage (line-to-line
voltage for Delta systems and line-to-neutral voltage for Wye systems).

 

Furthermore, there are a couple of notes around the ION Reference suggesting 3W-Wye may ignore the V2 input, and FA244106 seems to state this meter should be set up as Delta:  How can the PowerLogic meters monitor a 3 wire ungrounded WYE system | Schneider Electric USA

 

My question is, for a meter monitoring a network through a wye transformer using an HRG and no ground bus, what should the wiring type be and what should I set the nominal voltage to?

 

Thanks for your help!

Labels
  • Labels:
  • ION8000
  • ION9000
  • Power Quality
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-12-18 07:35 AM

0 Likes
0
1524
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
‎2024-12-18 07:35 AM

Hello @RobGraham 

3W-wye is not the volts mode you should be using. This is a very special configuration that is sometimes used in Utility type applications where a single CT to stepdown 100skV to 120V is worth more than the meter. In the install guide there is an image for the one and ONLY wiring that should be used with 3W-wye.

Charles_Murison_0-1734535880896.png


In your system, if the load is not connected to the same ground as the transformer to have a delta load, therefore I would suggest putting the meter into Delta mode. V nominal would be VL-L. If the load does have a ground connection, you will need to connect the same ground to the Vref(VN) of the meter. Volts mode would be 4W-wye and V nominal will be VL-N. 


Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 2
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-12-18 07:35 AM

0 Likes
0
1525
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
‎2024-12-18 07:35 AM

Hello @RobGraham 

3W-wye is not the volts mode you should be using. This is a very special configuration that is sometimes used in Utility type applications where a single CT to stepdown 100skV to 120V is worth more than the meter. In the install guide there is an image for the one and ONLY wiring that should be used with 3W-wye.

Charles_Murison_0-1734535880896.png


In your system, if the load is not connected to the same ground as the transformer to have a delta load, therefore I would suggest putting the meter into Delta mode. V nominal would be VL-L. If the load does have a ground connection, you will need to connect the same ground to the Vref(VN) of the meter. Volts mode would be 4W-wye and V nominal will be VL-N. 


Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
RobGraham
RobGraham Champion
Champion

Posted: ‎2024-12-18 08:57 AM

1 Like
0
1518
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
‎2024-12-18 08:57 AM

Thank you very much for a comprehensive solution!  I missed the wiring in the installation guide, and now I can confidently tell customers, "Don't use this.".
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.