Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION Setup now accepts restoring meter settings from register temporary files

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION Setup now accepts restoring meter settings from register temporary files
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
576
Mehran_Mehrnia
Mehran_Mehrnia Champion
215
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
sesa197217_brid
sesa197217_brid Contributor
Contributor

Posted: ‎2024-04-24 10:43 AM

0 Likes
4
1535
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
‎2024-04-24 10:43 AM

ION Setup now accepts restoring meter settings from register temporary files

While restoring a dcf template to an ION 9000 meter with ION Setup I've noticed there is a new option available to "Restore settings from previous paste".  This prompts for a .TMP Register temporary file, but I cannot find through the Setup Assistant menus or ION Setup's help files where this file can be created from.  Any insights are greatly appreciated.

a8699916-5c32-4af3-b8dd-e865e6e3badd.jpg

 

4b9586d8-72e3-4441-9cda-89cc5c686377.jpg

 

Labels
  • Labels:
  • ION Setup
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2024-04-25 11:40 AM . Last Modified: ‎2024-04-25 11:41 AM

1 Like
0
1467
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
‎2024-04-25 11:40 AM

When performing a normal template paste settings which you may want to retain that have already been set in the device are uploaded and stored in a temporary file (with a TMP extension).  This is the option shown in the dialog as Keep these settings as shown in your dialog.

If a template operation is successful, the temporary file is deleted automatically by ION Setup.

What occurs during the normal process is that those settings are read from the device and stored in a temporary file in a temp location.  Upgrade or template paste operation then begin and as a result the settings are reset in the device itself.  If for whatever reason, that operation would not complete, there was no way previously to somehow reuse the settings that are still stored in that temporary file (obviously uploading reset settings in the device again would be not desirable at all).

This new option would allow the user to bypass having to upload reset values, or just taking the ones in the template (which may not be applicable either) and selecting one from the previous failed operation (keep in mind this likely has to be done immediately as doing another similar operation will overwrite the same temporary file again).


See Answer In Context

Reply
Replies 4
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-04-24 03:33 PM

0 Likes
2
1510
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
‎2024-04-24 03:33 PM

Hello @sesa197217_brid ,

When first pasting a template, or upgrading a meter, when you select one or more settings to be saved, This primes PME what settings to save. Then before the template paste or firmware upgrade starts the .tmp file is saved in a temporary folder. If you look for %temp% in address bar you will find your temp folder. In this folder is one called ION Setup1 or just ION Setup. The .tmp file is saved to this folder and over written for each meter.

This file is only created just before pasting or upgrading a meter, When to see IOn Setup saying something like saving registers.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
sesa197217_brid
sesa197217_brid Contributor
Contributor

Posted: ‎2024-04-25 06:06 AM

0 Likes
1
1488
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
‎2024-04-25 06:06 AM

Thanks Charles, to clarify, can this only be taken advantage of if you're able to use both PME and ION Setup?  Also, is the .TMP file only created after an initial paste using the "Keep these settings on the device" option? 

 

When selecting the "Restore settings from a previous paste" option ION Setup does default to the "ION Setup 1" directory within the Temp folder.

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-04-25 08:50 AM

0 Likes
0
1479
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
‎2024-04-25 08:50 AM

Hello @sesa197217_brid ,

 

This is only ION Setup, PME does not come into play with this at all. Only ION Setup creates the file, only ION Setup can use the file. This is not a partial framework, this is specific settings for specific registers. The directory in the temp folder may be slightly different for your system. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2024-04-25 11:40 AM . Last Modified: ‎2024-04-25 11:41 AM

1 Like
0
1468
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
‎2024-04-25 11:40 AM

When performing a normal template paste settings which you may want to retain that have already been set in the device are uploaded and stored in a temporary file (with a TMP extension).  This is the option shown in the dialog as Keep these settings as shown in your dialog.

If a template operation is successful, the temporary file is deleted automatically by ION Setup.

What occurs during the normal process is that those settings are read from the device and stored in a temporary file in a temp location.  Upgrade or template paste operation then begin and as a result the settings are reset in the device itself.  If for whatever reason, that operation would not complete, there was no way previously to somehow reuse the settings that are still stored in that temporary file (obviously uploading reset settings in the device again would be not desirable at all).

This new option would allow the user to bypass having to upload reset values, or just taking the ones in the template (which may not be applicable either) and selecting one from the previous failed operation (keep in mind this likely has to be done immediately as doing another similar operation will overwrite the same temporary file again).
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.