Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hi, community.
Can somebody confirm if it’s possible to output the value of demand to the analog output module of the ION9000?
Our customer wants to confirm this before placing an order.
Thank you and Regards
Link copied. Please paste this link to share this article on your social media post.
Hello @XtianPilarcA ,
To the question, yes this can be done. The analog output module has a few setup registers that control how the input to the module affects the output as mentioned above. The one step not mentioned above is that the input to the analog output module needs to be linked to the desired Sliding window demand module's output. This can be done using ION Setup software. For more information on the analog output module refer to https://www.se.com/ca/en/download/document/7EN02-0290/.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi
Whats the demand range will be set? i.e Zero scale value & Full Scale value to drive Analog Output.
Whats type of application will be used? i.e ION9K Analog output will be connected to Analog Input for which device
In general, ION9K Analog Output (kW output can be used as Analog output) supports for applications to drive control valves.
Thanks & regards
Udhayakumar.A.K
Link copied. Please paste this link to share this article on your social media post.
Hello @XtianPilarcA ,
To the question, yes this can be done. The analog output module has a few setup registers that control how the input to the module affects the output as mentioned above. The one step not mentioned above is that the input to the analog output module needs to be linked to the desired Sliding window demand module's output. This can be done using ION Setup software. For more information on the analog output module refer to https://www.se.com/ca/en/download/document/7EN02-0290/.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
To what system do you want to share data? If SCADA I recommend using standard protocol like MODBUS or DNP 3 via meter communication ports.
To use the Analog out port send demand value I can confirm that this ION9000 is capable you need to add something in the framework.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.