ION 7330 through Ethertgate "ION7400" can not connect

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION 7330 through Ethertgate "ION7400" can not connect
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
525
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
138
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
PowerLogic
PowerLogic ION7400 series

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
JuanMQT
Lieutenant JG JuanMQT
Lieutenant JG

Posted: ‎2021-06-24 11:24 AM . Last Modified: ‎2024-01-30 04:42 AM

0 Likes
3
2306
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
‎2021-06-24 11:24 AM

ION 7330 through Ethertgate "ION7400" can not connect

Dear experts,

 

I have a costumer who wants to communicate his ION7330 through a ION7400 to a PME, its ION7330 has an ethernet port that is being used to report to a SCADA, acording to the manual the ION7330 supports a single Ethernet connection at a time. That's why we are trying through a gateway.

But I can not connect with the ION7330 

 

ION7330

ION7330 Baud rate.jpegION7330 ID.jpegION7330 Protocol.jpegION7330 Serial.jpeg

 

ION7400

ION7440 Gateway.jpegION7400.PNG

 

What should I do ?

  • Thumbnail of PowerLogic ION7400 series
    PowerLogic
    PowerLogic ION7400 series
View products (1)
Labels
  • Labels:
  • ION7000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Admiral Robert_Lee Admiral
Admiral

Posted: ‎2021-09-08 03:09 PM . Last Modified: ‎2021-09-08 03:43 PM

1 Like
0
2286
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
‎2021-09-08 03:09 PM

Does the ION7330 have a Modem installed (RJ-11 on the side of the unit).  If so, the Com1 RS-485 can only be used as an outgoing ModemGate port (allowing any communication via incoming modem calls to also talk to downstream devices) and can not be used to communicate to the device itself from the RS-485 side.  The Com2 port is also reserved for outgoing Ethergate operation if the meter is installed with Ethernet which you've indicated is being used by SCADA.

Unfortunately this only leaves the front optical port as the only means to communicate to the device if you can't use the modem to dial into the 7330 without disconnecting SCADA.

Another limited alternative would be to use the ION7400 to Modbus Master via TCP the ION7330 which would allow both SCADA and PME to connect to the ION7400 (since it supports multiple simultaneous connection and not just one like the 7330) but this limits the type of data retrieved to a limited set of real-time data.

If the unit does NOT have a modem port, then you should be able to communicate to the 7330 by using ION Setup, adding a gateway site using the ION7400 IP address and IP Port 7801, then adding an ION 7330 device to that site with a unit ID of 10.  Keep in mind that again only 1 software can connect to the Ethergate port so if ION Setup is connected, PME will not be able to at the same time.

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Replies 3
Charles_Murison
Picard Charles_Murison Picard
Picard

Posted: ‎2021-09-08 09:31 AM

0 Likes
0
2299
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
‎2021-09-08 09:31 AM

Hello @JuanMQT ,

 

I moved this post to the hardware forum. The settings and wiring look correct. Could try turning off the RS485 bias but I would not hold my breath that will fix the issue. Do you see activity lights on the ION7330 when you try to read? What software are you using to try connect with ION7330?

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
  • Tags:
  • english
Reply
Tom_Stevenson
Picard Tom_Stevenson Picard
Picard

Posted: ‎2021-09-08 10:46 AM

0 Likes
0
2293
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
‎2021-09-08 10:46 AM

Are you trying to connect via ION Setup or PME?  Is there any additional diagnostic information you are seeing (connection to ION7400 is ok, but serial timeouts to 7330?)

Tags (1)
  • Tags:
  • english
Reply
Robert_Lee
Admiral Robert_Lee Admiral
Admiral

Posted: ‎2021-09-08 03:09 PM . Last Modified: ‎2021-09-08 03:43 PM

1 Like
0
2287
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
‎2021-09-08 03:09 PM

Does the ION7330 have a Modem installed (RJ-11 on the side of the unit).  If so, the Com1 RS-485 can only be used as an outgoing ModemGate port (allowing any communication via incoming modem calls to also talk to downstream devices) and can not be used to communicate to the device itself from the RS-485 side.  The Com2 port is also reserved for outgoing Ethergate operation if the meter is installed with Ethernet which you've indicated is being used by SCADA.

Unfortunately this only leaves the front optical port as the only means to communicate to the device if you can't use the modem to dial into the 7330 without disconnecting SCADA.

Another limited alternative would be to use the ION7400 to Modbus Master via TCP the ION7330 which would allow both SCADA and PME to connect to the ION7400 (since it supports multiple simultaneous connection and not just one like the 7330) but this limits the type of data retrieved to a limited set of real-time data.

If the unit does NOT have a modem port, then you should be able to communicate to the 7330 by using ION Setup, adding a gateway site using the ION7400 IP address and IP Port 7801, then adding an ION 7330 device to that site with a unit ID of 10.  Keep in mind that again only 1 software can connect to the Ethergate port so if ION Setup is connected, PME will not be able to at the same time.

Tags (1)
  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.