Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

How to solve error "Meter framework missing required configuration register" shown in ION SETUP

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • How to solve error "Meter framework missing required configuration register" shown in ION SETUP
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
Ezequiel-PROLUX
Ezequiel-PROLUX
Contributor

Posted: ‎2017-11-07 03:23 AM . Last Modified: ‎2020-04-22 01:15 AM

0 Likes
2
1421
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
‎2017-11-07 03:23 AM

How to solve error "Meter framework missing required configuration register" shown in ION SETUP

Hi guys,

We are in the field testing some ION8600 meters, and one shows up with that error when clicked button SCALING in TEST MODE.

meter framework missing.png

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-11-09 11:03 PM

1 Like
1
1400
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
‎2017-11-09 11:03 PM

The dialog is being displayed due to the fact that the button is tied to a specific register which on that particular 8600 is not present in the template or has been moved to a different register.

Looking at a default 8600 template this should be External Boolean #29 (Scale Tst Mode), so if this module doesn't exist or the template has it moved elsewhere, you will need to either need to customize the setup assistant to match it or the better solution is to put it back as External Boolean #29.

Customization of frameworks which aren't done properly without corresponding changes in the Setup Assistant will cause numerous other issues, so tread carefully when deleting or moving modules from their default functionality.

See Answer In Context

Reply
Replies 2
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-11-09 11:03 PM

1 Like
1
1400
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
‎2017-11-09 11:03 PM

The dialog is being displayed due to the fact that the button is tied to a specific register which on that particular 8600 is not present in the template or has been moved to a different register.

Looking at a default 8600 template this should be External Boolean #29 (Scale Tst Mode), so if this module doesn't exist or the template has it moved elsewhere, you will need to either need to customize the setup assistant to match it or the better solution is to put it back as External Boolean #29.

Customization of frameworks which aren't done properly without corresponding changes in the Setup Assistant will cause numerous other issues, so tread carefully when deleting or moving modules from their default functionality.

Reply
Ezequiel-PROLUX
Ezequiel-PROLUX
Contributor

Posted: ‎2017-11-13 02:46 AM

0 Likes
0
1400
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
‎2017-11-13 02:46 AM

Thank you!

That information is exactly what we needed.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.