Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

How to change an external numeric variable in a custom webpage of a PM8000 or Ion9000

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • How to change an external numeric variable in a custom webpage of a PM8000 or Ion9000
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Erwin_Paal
Erwin_Paal Mentor
Mentor

Posted: ‎2022-03-31 01:33 AM

0 Likes
4
2644
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
‎2022-03-31 01:33 AM

How to change an external numeric variable in a custom webpage of a PM8000 or Ion9000

For small framework applications (switching off via some kind of max power, more complex semaphore alarming...) it is very helpful for end users to set the setpoint parameters via a user defined web page.


Using the ION setup is not an option and customers without PME have no other choice.

 

As described in the manual, you can create custom setup webpages.
However, according to the mapping list, the external variables do not have Web Page Tag (have not been defined), so unfortunately you cannot use the syntax:
<td><input name="Web Page Tag Name" type="text" /></td>
Have tried to use here instead of the Web page tag, the ION handle (regname=”_0x####”), unfortunately it does not work. Can only able to see (read) the values.

Is it not possible to use the ION handle here to?

If so, how could the syntax look like?

 

Thanks!

Labels
  • Labels:
  • ION9000
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Erwin_Paal
Erwin_Paal Mentor
Mentor

Posted: ‎2022-04-27 08:11 AM

1 Like
0
2367
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
‎2022-04-27 08:11 AM

Hello Charles!

We are looking for a solution via the meter's web page, so ideally via the Custom web page.

 

A workaround via additional tools (Modbus tool, ION Setup) to write the parameters via Modbus is unfortunately not useful and also not easy for the customer. Why do we have the setting page on the meter?

 

Solution, as a workaround, I already have via ION Setup. See the .pml files in the attachment

Copy the .pml files for example into the installation folder of the ION Setup: "C:\Program Files (x86)\Schneider Electric\ION Setup\Tables\PM8000\Version 5.1 Default".
With this you can set the parameters in the ION Setup, here screenshot:

Screenshot 1.JPGScreenshot 2.JPG

 

See Answer In Context

Attachments
Enables External Variables.zip
Tags (1)
  • Tags:
  • english
Reply
Replies 4
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2022-04-18 08:44 AM . Last Modified: ‎2022-04-18 11:47 AM

0 Likes
3
2489
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
‎2022-04-18 08:44 AM

Hello @Erwin_Paal ,

 

Short answer is correct, not able to do the control you desired. Note that the external numeric/Boolean/Pulse registers do have a default modbus address, you may be able to do what you are looking for with modbus read/write commands.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
  • Tags:
  • english
Reply
DanL
DanL Champion
Champion

Posted: ‎2022-04-18 06:09 PM

0 Likes
1
2466
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
‎2022-04-18 06:09 PM

FYI: @Daniel_Brandao It looks like this feature was available in web pages for firmware v2.1 and earlier

Tags (1)
  • Tags:
  • english
Reply
Anonymous user
Not applicable

Posted: ‎2022-04-27 05:06 AM

0 Likes
0
2376
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
‎2022-04-27 05:06 AM

This works really well for us, thank you! Facing same issue here. Help is appreciated.

Tags (1)
  • Tags:
  • english
Reply
Erwin_Paal
Erwin_Paal Mentor
Mentor

Posted: ‎2022-04-27 08:11 AM

1 Like
0
2368
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
‎2022-04-27 08:11 AM

Hello Charles!

We are looking for a solution via the meter's web page, so ideally via the Custom web page.

 

A workaround via additional tools (Modbus tool, ION Setup) to write the parameters via Modbus is unfortunately not useful and also not easy for the customer. Why do we have the setting page on the meter?

 

Solution, as a workaround, I already have via ION Setup. See the .pml files in the attachment

Copy the .pml files for example into the installation folder of the ION Setup: "C:\Program Files (x86)\Schneider Electric\ION Setup\Tables\PM8000\Version 5.1 Default".
With this you can set the parameters in the ION Setup, here screenshot:

Screenshot 1.JPGScreenshot 2.JPG

 

Attachments
Enables External Variables.zip
Tags (1)
  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.