Accepted Solutions
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
James,
The PM5560 supports 128 concurrent TCP/IP Ethernet connections, these are used for HTTP, FTP, Modbus TCP and other protocols.
The maximum concurrent HTTP connections is 20.
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
That's great news! Can you be more specific about the PM5320 and PM5340 with Ethernet? You mention the PM5560, but what about the others?
What's the maximum Modbus TCP connections?
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
I will let Shreesha Pandith respond about the PM5320 and PM5340, he is closer to that
development.
From: James DiLiberto <powersolutionscommunity-admin@powersolutionscommunity.hosted.jivesoftware.com>
To: Marcelo Perez <marcelo.perez@schneider-electric.com>,
Date: 02/10/2014 06:28 PM
Subject: Re: - How many concurrent Modbus TCP connections are allowed on the PM5000
series meters with Ethernet?
Solutions Expert Community
How many concurrent Modbus TCP connections are allowed on the PM5000 series meters with
Ethernet?
reply from James DiLiberto in Power Monitoring Hardware - View the full discussion
That's great news! Can you be more specific about the PM5320 and PM5340 with Ethernet? You
mention the PM5560, but what about the others?
What's the maximum Modbus TCP connections?
Reply to this message by replying to this email, or go to the message on Solutions Expert
Community
Start a new discussion in Power Monitoring Hardware by email or at Solutions Expert Community
Following How many concurrent Modbus TCP connections are allowed on the PM5000 series meters
with Ethernet? in these streams: Inbox
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
Hi, How about the PM8ECC module ?