Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
I have a PM8000 installed upon a 11kV system which is monitoring the voltage using 11000/110V PTs.
The meter has been configured using ION Setup 3.1 as follows:
PT Primary: 11000V
PT Secondary: 110V
Nominal Voltage 11000V
When I close the connection between ION Setup and the meter, the Device Configuration Checklist > Configuration Warnings states: PT primary/nominal mismatch". Why is this when the two are the same value?
Link copied. Please paste this link to share this article on your social media post.
What volts mode do you have the device operating in?
If the system is operating in a Delta system, the existing version of ION Setup has a problem in that it is mistakenly expecting the Vnominal to be root3 times as big (plus/minus 10%) instead of just being in the ballpark.
Next version will have this issue corrected.
Link copied. Please paste this link to share this article on your social media post.
What volts mode do you have the device operating in?
If the system is operating in a Delta system, the existing version of ION Setup has a problem in that it is mistakenly expecting the Vnominal to be root3 times as big (plus/minus 10%) instead of just being in the ballpark.
Next version will have this issue corrected.
Link copied. Please paste this link to share this article on your social media post.
The system is set up as Delta.
Thank you for the response.
@Anonymous user
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.