Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Introducing the latest release of firmware version 4.6.0 for the PowerLogic™ Advanced Meters. This update brings several significant enhancements to improve functionality and security. Here are the top changes found in the latest firmware:
Upgrade to firmware version 4.6.0 today to take advantage of these powerful new features.
Please find the download links for firmware below:
https://www.se.com/us/en/download/document/ION9000_meter_FW_v004_006_000/
https://www.se.com/us/en/download/document/ION7400_meter_FW_v004_006_000/
https://www.se.com/us/en/download/document/PM8000_meter_FW_v004_006_000/
Additional Documentation:
BACnet Certificate: Download
Link copied. Please paste this link to share this article on your social media post.
Thank you for the information and for sharing the new update on FW V4.6.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
The new update does not enable me to add the meter on Ecostruxure Power Commission project, from EPC version 2.35 to 2.36. This is concerning the PM8210 meters, when the firmware version is reverted to 004.005.00, the power meter can be added to a project. Please assist
Link copied. Please paste this link to share this article on your social media post.
Hello @Chief2403 ,
In V4.6.0 Firmware, the function code 43 behavior was changed to allow for new meters to provide additional information. This change will make existing meters not return information in the same place EPC is currently using. EPC team is aware and firmware team is working with them.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Ok thanks for the update and with regard to PM5580 and PM5560, some of the meters do not show the normal webpage interface and thus the default username and passwords don't work. I have tried updating them to 4.4.5 from version 4.3.2. Some allow and some don't. What could be the cause?
Kind Regards
Chief Choshane
Link copied. Please paste this link to share this article on your social media post.
Hello @Chief2403 ,
Recommend to start a new topic on this question rather than reply to a topic unrelated to PM5000 series of meters.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Is there a hardware limitation of meters that can be upgraded to 4.6.0? Also, I know that for meters with FW 1.4.3 or bellow we first have to upgrade to 2.1.0>4.0.0>4.5.0 (can I go directly to 4.6.0 or do I have to upgrade first to 4.5.0?
Link copied. Please paste this link to share this article on your social media post.
Hi @bhernandez
The upgrade path V1.4.3 -> V2.1 -> V3.1 or V4.0.0 or V4.5.0 or V4.6.0(which is the latest) is correct as long as firmware version 2.1.0 have been previously installed and ensure using the latest version of Install ION Setup when upgrading to V4.6 (v3.2.25037.01 or higher). The current version is v3.2.251185.01 .
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Thank you for the quick response @Mehran_Mehrnia
Regarding the hardware version, can any ION7400 meter handle the latest firmware?
For example, is there no hardware version restriction related to the last two digits of the serial number (e.g., "-01", "-02", etc.)?
Link copied. Please paste this link to share this article on your social media post.
Hi @bhernandez
You're welcome.
There shouldn't be any restrictions based on hardware versions, as far as I'm aware. However, starting with firmware version 4.5, a new 'Feature Set' classification was introduced, Essential, Standard, and Advanced which determines the meter's capabilities based on firmware.
The feature set is selected at the time of purchase. All devices purchased before the release of firmware version 4.5.0 are assigned the Standard feature set by default. Therefore, when upgrading the meter, please ensure that you select the appropriate firmware template that matches the meter’s feature set.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Hi,
is this new firmware version compatible with a version of PME?
(I had issues before regarding this)
AND can`t find any documentation regarding ION setup and choosing Template option in PM8243:
I thought that firmware version in the meter has to be linked to the right template option in ION setup?
--> But there is also version 5.0 Default and 5.1
What do I chose, and where can I find documentation regarding this?
What is the difference regarding Advanced V4.6.0 vs Standard V4.6.0?
BR
GIA
Link copied. Please paste this link to share this article on your social media post.
As mentioned in previous post above, starting with firmware version 4.5, a new 'Feature Set' classification was introduced, Essential, Standard, and Advanced which determines the meter's capabilities based on firmware.
PM8000 Overview -> Feature Set
The 'Template Options' allow you to select which template ION Setup uses to display and configure data. This selection is based on the meter's firmware version, its feature set, and the corresponding compatible template. In this case, the available options include:
Standard V4.6.0 Default
Advanced V4.6.0 Default
As mentioned in PM8000 User guide, PM8243 is a DIN Rail meter with Standard feature set.
For PME compatibility, the PME team would be best suited to assist you. However, I believe the Vista diagram in PME may need to be updated.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Hi
If the ION9000 and ION7400 can now record up to 50 connected sources in the data logs, when a tabular report is downloaded in PME, will it be possible to generate a single report with all 50 sources?
BR
Diego Macario
Ecoxpert Master Digital
Link copied. Please paste this link to share this article on your social media post.
Hello @diego_macario_m ,
No, PME tabular reports and meters Data Recorders are separate development teams. Would need to request the feature to PME team through Schneider sales channels.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
hola @Charles_Murison,
quisiera comentarle que tube un problema actualizando al firmware v4.00.6.000, ahora me solicita usuario y password para todo, he intentado con los usuarios y password por defecto pero no funciona nada, es un ION7400
Link copied. Please paste this link to share this article on your social media post.
Hello @Osvaldo1704 ,
Advanced security was a requirement starting in V3.0.0 Firmware. I suggest reaching out to your local technical support to start a support case.
Regards,
Charles
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.