Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

EM49xx Setup & Configuration

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EM49xx Setup & Configuration
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
johannvd
johannvd
Contributor

Posted: ‎2024-06-04 04:44 AM

0 Likes
1
1644
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
‎2024-06-04 04:44 AM

EM49xx Setup & Configuration

Good day,

 

An existing installation of an EM4900 multi-circuit meter required monitoring of additional circuits.

Existing install had Channel 1 - 20 all as single phase and 21-23 & 24-26 as three phase connections.

 

CT's was installed and connected to channels 27, 28 and 29 and meter was setup using ION Setup on the following screens:

  1. Branch Circuit Sizes
  2. Breaker Sizes
  3. Logical Mater Setup

The meter itself was also restarted as the default Operating_Mode  is 1 (Discovery) and is required to detect configuration changes but I believe this is related to BACnet which is not being used as the meter is connected to a PME.

 

The issue we are facing is that the meter does not display the correct Amp readings for any of the three new CTs installed. One of the CT outputs were measured using a multimeter and we did pick up a reading.

 

I've gone through the following document but could not find any information as to what might be the cause or the solution. 

 

Any help will be appreciated.

 

Thanks,

Johann

Labels
  • Labels:
  • HDPM6000
  • ION Setup
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
johannvd
johannvd
Contributor

Posted: ‎2024-06-19 07:20 AM . Last Modified: ‎2024-06-19 07:22 AM

0 Likes
0
1494
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
‎2024-06-19 07:20 AM

Just to close the loop on this.

 

Upon closer review of the configuration and actually intending to move some of the CT's around to ensure that all single phase connections are grouped prior to any three phase connection I realized the CT configuration was incorrect.

For the 2 x three phase connections the CT configuration is to be done on all the channels. This is a bit in contrast to a "normal" three phase meter where the CT ratio is only configured once and this is where the previous configuration was incorrect. I basically took the existing configuration as correct and just added the three new CT's at the end of the list.

Once the meter was reconfigured on all CT channels regardless of single- of three-phase the readings came through correctly (verified) for the new circuits and was also corrected on the two three-phase connections as well although the readings were extremely low on these connections.

 

See Answer In Context

Reply
Reply 1
johannvd
johannvd
Contributor

Posted: ‎2024-06-19 07:20 AM . Last Modified: ‎2024-06-19 07:22 AM

0 Likes
0
1494
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
‎2024-06-19 07:20 AM

Just to close the loop on this.

 

Upon closer review of the configuration and actually intending to move some of the CT's around to ensure that all single phase connections are grouped prior to any three phase connection I realized the CT configuration was incorrect.

For the 2 x three phase connections the CT configuration is to be done on all the channels. This is a bit in contrast to a "normal" three phase meter where the CT ratio is only configured once and this is where the previous configuration was incorrect. I basically took the existing configuration as correct and just added the three new CT's at the end of the list.

Once the meter was reconfigured on all CT channels regardless of single- of three-phase the readings came through correctly (verified) for the new circuits and was also corrected on the two three-phase connections as well although the readings were extremely low on these connections.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.