Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

EM4200 Live Data Table

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EM4200 Live Data Table
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
michael_franz
michael_franz
Mentor

Posted: ‎2017-07-14 06:26 AM . Last Modified: ‎2020-04-22 01:15 AM

0 Likes
3
2907
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
‎2017-07-14 06:26 AM

EM4200 Live Data Table

ION Setup has an entry for this meter but appears to be lacking live data table for this type.

 

This is .16xxxx that we had believed to be the newest.

EM4200.jpg

 

 

Found .17xxxx and at least we do not get the "no tables found" error.  Won't know if this is the

fix until we can connect to a meters.

Attachments
Labels
  • Labels:
  • ION Setup
Tags (5)
  • Tags:
  • data
  • em4200
  • ion setup
  • live data
  • meter
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-07-18 12:04 PM

1 Like
1
2882
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
‎2017-07-18 12:04 PM

I believe what is happening is that ION Setup is presently trying to use the wrong folder names since the EM4200 is a somewhat new product.  It is automatically talking to the device and instead of picking the "EM4235" folder which is what ION Setup installed, it is selecting "Enhanced" (which is left over from the older Enercept implementation).  Likewise the "EM4236" is selecting the "Basic" instead.

For now you should can select the Display tab and manually select the proper model (make sure either the EM4235 or EM4236 is highlighted) or if that doesn't work, using Windows Explorer, create copies of the existing folders and rename them appropriately (ex. copy of the EM4235 folder call it "Enhanced").

I will try and update ION Setup to select the proper folders in the next release.

See Answer In Context

Reply
Replies 3
michael_franz
michael_franz
Mentor

Posted: ‎2017-07-17 07:38 AM

0 Likes
0
2882
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
‎2017-07-17 07:38 AM

TEAM:

No takers on this???  ION Setup is an important tool.  We need those tables.

Thanks,

Michael Franz

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-07-18 12:04 PM

1 Like
1
2882
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
‎2017-07-18 12:04 PM

I believe what is happening is that ION Setup is presently trying to use the wrong folder names since the EM4200 is a somewhat new product.  It is automatically talking to the device and instead of picking the "EM4235" folder which is what ION Setup installed, it is selecting "Enhanced" (which is left over from the older Enercept implementation).  Likewise the "EM4236" is selecting the "Basic" instead.

For now you should can select the Display tab and manually select the proper model (make sure either the EM4235 or EM4236 is highlighted) or if that doesn't work, using Windows Explorer, create copies of the existing folders and rename them appropriately (ex. copy of the EM4235 folder call it "Enhanced").

I will try and update ION Setup to select the proper folders in the next release.

Reply
michael_franz
michael_franz
Mentor

Posted: ‎2017-07-18 12:08 PM

0 Likes
0
2882
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
‎2017-07-18 12:08 PM

Robert Lee:

I had 3.0.16xxxxx that had claimed to be the newest.  Got a link for 3.0.17xxxxx

that looks like it will work.

Thanks,

Michael
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.