Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Is it possible to create a software program using the Power Monitoring Expert software that computes energy consumption when either the generator power or the main line is utilized, leveraging a single power meter?
The program should account for dynamic usage patterns(of the generator power whenever there is a power cut) rather than following a predetermined schedule. Subsequently, these computed values(Mains and Generator power) will be used to generate a billing report that incorporates two distinct energy rates.
Link copied. Please paste this link to share this article on your social media post.
Hello @ajith_iqsystems ,
In the world of ION there is usually more than 1 way to do things. For example, if you are able to link a status, utility vs generator, to a digital input, you could build a framework that can activate or deactivate modules like integrator modules that can calculate energy from power. Or you could log the status along with energy and calculate the approximate usage. Just logging the status would give you a resolution of the logging interval so would not be as accurate as calculating different energies under different input conditions.
As for the billing, you may need to use the billing report to be able to have the different rates for the different energy sources.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi @Charles_Murison ,
Could the functionalities described above, such as linking a status between a utility vs generator to a digital input for activating or deactivating modules like integrator modules, and calculating energy from power, be implemented using the EM1000 and PM2120 power meters?
Could you please guide us to create a program to calculate separately utility usage and generator usage monthly. And this calculated consumption need to be mapped to the bill and assigned 2 separate rates for each consumptions.
Link copied. Please paste this link to share this article on your social media post.
Hello @ajith_iqsystems ,
I have not worked with EM1000 and PM2120 meters so I cannot say what they are capable of.
Regarding the framework and setting up the billing report. I can give you general ideals but not specifics. There may be others in the forums that could possibly offer that service (likely with a fee).
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.