Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Dual Modbus Port (RTU & TCP/IP) Slave with Dual Modbus Master.

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Dual Modbus Port (RTU & TCP/IP) Slave with Dual Modbus Master.
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa102505_brid
sesa102505_brid Explorer
Explorer

Posted: ‎2017-08-30 07:48 PM

0 Likes
2
1554
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
‎2017-08-30 07:48 PM

Dual Modbus Port (RTU & TCP/IP) Slave with Dual Modbus Master.

Hi, can I connect into a PM5560 two gateways actin as master devices? First connected by RS-485 and the second at Modbus TCP/IP ?

Is there any guidance by product line, like 5000 series / 8000 series?

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Anonymous user
Not applicable

Posted: ‎2017-08-31 05:12 AM

1 Like
1
1523
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
‎2017-08-31 05:12 AM

Hi Evandro,

Connecting a gateway to the Ethernet port doesn't make sense. A gateway converts protocols on the OSI layers e.g. Modbus RTU (RS485 serial) to Modbus TCPIP (Ethernet) - or - BACnet RTU to BACnet IP

I'm not sure whether this will work, it is usually one method or the other, not both. I have not tried it but someone else on the Exchange may have...

Yes, you can have multiple masters on a serial line poll a slave device; however, you may lose packets if both masters try and poll at the same time, limit time between requests from the masters. In your case, the solution may be to connect another gateway to the serial line?

Hope this helps.

Reply
sesa102505_brid
sesa102505_brid Explorer
Explorer

Posted: ‎2017-08-31 04:01 PM

0 Likes
0
1523
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
‎2017-08-31 04:01 PM

Hi, the scenario is a little bit different.

Customer needs to monitor the energy into two different systems, that cannot share the same ethernet network.

So the idea was to MAP this electrical meter at a existing Quantum PLC, and map the same electrical meter in a COMX for a WAGES project.

Doing this way, he will keep with the premises, not to connect WAGES project at the industrial network.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.