Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

DNP3 ION METER 8650 polling data issue

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • DNP3 ION METER 8650 polling data issue
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa427872_brid
sesa427872_brid Explorer
Explorer

Posted: ‎2019-01-18 02:03 PM . Last Modified: ‎2020-04-22 01:02 AM

0 Likes
2
2856
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
‎2019-01-18 02:03 PM

DNP3 ION METER 8650 polling data issue

i am using RTU to collect data from ION8650  throuh dnp3 and i face problem in retriveing data in rtu (no change happens in rtu ) so i checked my configuration and i found that unsolenable parameter is temperary disapled and can not change it .

 

any advise to enable this function 

Attachments
Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2019-01-22 10:43 AM . Last Modified: ‎2019-01-22 10:49 AM

0 Likes
0
2852
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
‎2019-01-22 10:43 AM

The DNP Slave Option setup register "Unsolicated Response" is an unfinished firmware feature which has not yet been prioritized for implementation.  We had intended to implement it at a future date but there hasn't been a firm need so this has never been completed.

 

That however, is unlikely to be the source of the DNP comm issue you are experiencing.  If you are using DNP over a serial connection, you also need to select the "DNP 3.0" protocol for the intended Comm Port you are using AFTER you enable the DNP Slave Option Comm Port setup register as well (you will still need to do the latter even if you are communicating DNP over TCP).  I would suggest using the DNP Assistant in ION Setup to enable the DNP as it will help perform most of the needed tasks.

 

As for the DNP implementation on the firmware, we presently use the ASE2000 test set to confirm our DNP implementation for all our ION products and I believe they have a demo version which is time/feature limited which you might be able to check the communications.

See Answer In Context

Reply
Replies 2
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2019-01-22 10:43 AM . Last Modified: ‎2019-01-22 10:49 AM

0 Likes
0
2852
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
‎2019-01-22 10:43 AM

The DNP Slave Option setup register "Unsolicated Response" is an unfinished firmware feature which has not yet been prioritized for implementation.  We had intended to implement it at a future date but there hasn't been a firm need so this has never been completed.

 

That however, is unlikely to be the source of the DNP comm issue you are experiencing.  If you are using DNP over a serial connection, you also need to select the "DNP 3.0" protocol for the intended Comm Port you are using AFTER you enable the DNP Slave Option Comm Port setup register as well (you will still need to do the latter even if you are communicating DNP over TCP).  I would suggest using the DNP Assistant in ION Setup to enable the DNP as it will help perform most of the needed tasks.

 

As for the DNP implementation on the firmware, we presently use the ASE2000 test set to confirm our DNP implementation for all our ION products and I believe they have a demo version which is time/feature limited which you might be able to check the communications.

Reply
Anonymous user
Not applicable

Posted: ‎2019-08-22 08:25 AM

0 Likes
0
2827
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
‎2019-08-22 08:25 AM

Hi @sesa427872_brid,

 

@Robert_Lee  helped you to solve your problem. Please click on “Accept as Solution” so other members can find the same solution through the search bar. Thank you!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.