Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Config communication PM8000

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Config communication PM8000
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
570
Mehran_Mehrnia
Mehran_Mehrnia Champion
200
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-03-28 04:05 AM

1 Like
21
9255
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
‎2019-03-28 04:05 AM

Config communication PM8000

Hi teams,

 

I have concern, i want configure in communication of  2 PM8000, 1 slave and 1 master as image below.

 

How do i do in PM8000? Thanks very much

 

This is my configure in PM8000. Do i it right or wrong?

 

Image 0: Architecture 

TH1.png

 

Image 1: Config PM8000 is Master

 

PM8000 Master_TH1.JPG

 

 

Image 2: Config PM8000 is Slave

 

PM8000 Slave_TH2 vs TH1.JPG

 

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-03-28 11:18 AM

0 Likes
1
9233
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
‎2019-03-28 11:18 AM

rest of the settings look good.

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-04-01 09:27 AM . Last Modified: ‎2019-04-01 09:36 AM

0 Likes
6
9211
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
‎2019-04-01 09:27 AM

The PM8000 has 2 different ways to be a gateway

Ethergate: 

Ethernet connected meter, Com Protocol: Ethergate 

Connect to the meter on port 7801, only 1 connection at a time. Can be either ION or Modbus, depends on the setting of RS485 meter and the software connecting to the meter. Recommended only 1 protocol on the RS-485 loop, not recommended mix ION and mosbus.

 

Modbus gateway:

Ethernet connected meter,

Com Protocol: Modbus Master   

Modbus master option module, Serial connection 1 -> Comm1  Gateway enabled and serial connection 1 selected

RS-485 Meter com protocol has to be Modbus.

Multiple connections to the gateway meter possible on port 502. One big downside is that the RS-475 meter does not have access to logged values, waveforms etc when using Modbus.

 

If using PME to talk to the RS-485 meter. STRONGLY recommend using ethergate, as no default drive to talk modbus to the PM8000 in PME.

 

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-05-08 10:32 AM

0 Likes
2
9182
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
‎2019-05-08 10:32 AM

Hi @Yut ,

 

Because my customer hard supply IP. So, we just need 01 PM8000 is Ethergate, 08 PM8000 will slave with modbus RS485

 

Hic.

See Answer In Context

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-05-21 08:29 AM . Last Modified: ‎2019-05-22 11:24 AM

0 Likes
1
9160
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
‎2019-05-21 08:29 AM

Modbus master is used 1 for 2 possible conditions, 1, the meter is modbus mastering the slave devices itself, or 2, the meter is acting as a modbus gateway only, no other protocol is able to talk to downstream devices. Many features of the PM8000 meter are only avalaiable to the ION Protocol especially when using PME so I DO NOT recommend using modbus for the downstream device.

 

Ethergate is able to transfer the ION requests from Ethernet to serial and then back to ethernet to PME. Port 7801 is only used with Ethergate and the meter can only use 1 setting for the serial side. You will still only use 1 IP address but it will be duel function, 1 device is an ethernet device, the downstream device is a serial device on ethernet gateway.

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Yut
Yut
Leader

Posted: ‎2019-05-23 09:40 PM

0 Likes
1
9147
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
‎2019-05-23 09:40 PM

You can use the first PM8000 as gateway using ION protocol.

See Answer In Context

Reply
Replies 21
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-03-28 08:55 AM

0 Likes
5
9252
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
‎2019-03-28 08:55 AM

Com 1 Serial port between the 2 meters do not match, Master is 8E2, slave is 8N1. Both need to match.

L4 Prime for Advanced metering and Utilities
Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-03-28 09:12 AM

0 Likes
4
9249
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
‎2019-03-28 09:12 AM

Hi Charles,

 

Thanks you. I will revise.

 

I will configure as follows:

 

 - PM8000 is master:

                                  + COM1 Protocol: EtherGate

                                  + COM 1 Baud rate: 9600

                                  + COM1 Timeout: 3.000

                                  + COM1: Unit ID: 1

                                  + COM1: Serial port: 8E2

                                  + COM1: RS485 Bias: ON

 

- PM8000 is Slave:   

                                  + COM1 Protocol: ION

                                  + COM 1 Baud rate: 9600

                                  + COM1 Timeout: 3.000

                                  + COM1: Unit ID: 3

                                  + COM1: Serial port: 8E2

                                  + COM1: RS485 Bias: ON

 

Is the configure correct?

 

 

 

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-03-28 09:15 AM

0 Likes
3
9245
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
‎2019-03-28 09:15 AM

Hello,

 

If you can do faster than 9600 baud rate without communications issues I would suggest that 19.2k is pretty common. On the slave meter I would disable the RS485 Bias.

L4 Prime for Advanced metering and Utilities
Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-03-28 09:25 AM

0 Likes
2
9240
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
‎2019-03-28 09:25 AM

Hi Charles,

 

Yes. Thanks Charles. I know and i also want use Baud rate 19,2k. But, My customer PME system use 9200 because their system unstable.

 

I will disable RS485 bias at slave meter.

 

And the rest in this setting it ok? Thanks Charles

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-03-28 11:18 AM

0 Likes
1
9234
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
‎2019-03-28 11:18 AM

rest of the settings look good.

L4 Prime for Advanced metering and Utilities
Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2019-03-28 02:19 PM . Last Modified: ‎2019-03-28 02:27 PM

0 Likes
8
9231
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
‎2019-03-28 02:19 PM

Question I have is the PM8000 the only slave device on the RS-485?  If there are other Modbus device on the same loop, you will likely need to reconfigure the protocols and move to Modbus Gateway which uses Modbus Master (instead of Ethergate) on the gateway PM8000 and Modbus RTU (instead of ION) on the slave PM8000.  You would also need to set the Modbus Gateway to COM1 via ION Setup (Basic Ethernet -> TCP/IP tab).  You will also need recent PM8000 firmware and PME in order to support ION over Modbus in order to operate in this manner.  We do not recommend mixing ION devices using ION protocol with Modbus-based devices on the same RS-485.

If there are only ION meters on the RS-485, then what you have shown is correct (although your original diagram Image 0: Architecture indicated Modbus protocol and not ION).

 

Also you will be restricted to a single master (PME by the looks of it) to communicate to the slave PM8000 (i.e. trying to use another application like ION Setup will result it in not able to connect to the Ethergate port of 7801 while PME is connected).

Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-03-30 08:47 AM

0 Likes
7
9215
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
‎2019-03-30 08:47 AM

Hi Robert,

 

Thanks you. Yes. The only PM8000 slave device in loop RS485.

 

So, my architecture is correct?. My customer only read value fundamential: I, V, P, E.

 

Thanks Robert.

 

Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-03-30 08:48 AM

0 Likes
0
9213
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
‎2019-03-30 08:48 AM

Hi Charles,

 

Thanks for your support. 

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-04-01 09:27 AM . Last Modified: ‎2019-04-01 09:36 AM

0 Likes
6
9212
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
‎2019-04-01 09:27 AM

The PM8000 has 2 different ways to be a gateway

Ethergate: 

Ethernet connected meter, Com Protocol: Ethergate 

Connect to the meter on port 7801, only 1 connection at a time. Can be either ION or Modbus, depends on the setting of RS485 meter and the software connecting to the meter. Recommended only 1 protocol on the RS-485 loop, not recommended mix ION and mosbus.

 

Modbus gateway:

Ethernet connected meter,

Com Protocol: Modbus Master   

Modbus master option module, Serial connection 1 -> Comm1  Gateway enabled and serial connection 1 selected

RS-485 Meter com protocol has to be Modbus.

Multiple connections to the gateway meter possible on port 502. One big downside is that the RS-475 meter does not have access to logged values, waveforms etc when using Modbus.

 

If using PME to talk to the RS-485 meter. STRONGLY recommend using ethergate, as no default drive to talk modbus to the PM8000 in PME.

 

L4 Prime for Advanced metering and Utilities
Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-04-04 12:17 PM

0 Likes
0
9201
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
‎2019-04-04 12:17 PM

Hi Charles,

 

Thanks Charles.

Reply
Yut
Yut
Leader

Posted: ‎2019-05-08 12:55 AM

0 Likes
3
9189
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
‎2019-05-08 12:55 AM

Why MODBUS you can get most of PM8000 with PME using ION Protocol ?

Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-05-08 10:32 AM

0 Likes
2
9183
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
‎2019-05-08 10:32 AM

Hi @Yut ,

 

Because my customer hard supply IP. So, we just need 01 PM8000 is Ethergate, 08 PM8000 will slave with modbus RS485

 

Hic.

Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-05-16 08:53 PM

0 Likes
4
9173
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
‎2019-05-16 08:53 PM

Hi @Charles_Murison @Yut ,

 

I was configure for the first PM8000 is Master (Modbus master) and the second PM8000 is slave look like image below.

 

Settinng for masterSettinng for masterSetting for SlaveSetting for SlaveSetting in PMESetting in PME

But when i configure in PME. I can't reveive data. Pls see and recommend for me if i wrong setting.

 

Thanks very much

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-05-17 10:12 AM

0 Likes
3
9167
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
‎2019-05-17 10:12 AM

On the  PM8000 is Master, change the port 1 protocol to Ethergate.

L4 Prime for Advanced metering and Utilities
Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-05-19 03:00 AM

0 Likes
2
9165
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
‎2019-05-19 03:00 AM

Hi @Charles_Murison ,

 

Thanks for your information. But why PM8000 port 1 replace from Modbus Master to Ethernet Gateway?

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-05-21 08:29 AM . Last Modified: ‎2019-05-22 11:24 AM

0 Likes
1
9161
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
‎2019-05-21 08:29 AM

Modbus master is used 1 for 2 possible conditions, 1, the meter is modbus mastering the slave devices itself, or 2, the meter is acting as a modbus gateway only, no other protocol is able to talk to downstream devices. Many features of the PM8000 meter are only avalaiable to the ION Protocol especially when using PME so I DO NOT recommend using modbus for the downstream device.

 

Ethergate is able to transfer the ION requests from Ethernet to serial and then back to ethernet to PME. Port 7801 is only used with Ethergate and the meter can only use 1 setting for the serial side. You will still only use 1 IP address but it will be duel function, 1 device is an ethernet device, the downstream device is a serial device on ethernet gateway.

L4 Prime for Advanced metering and Utilities
Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-05-22 09:59 AM

0 Likes
0
9154
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
‎2019-05-22 09:59 AM

Hi @Charles_Murison ,

 

Sincerely, Thanks for your information. I'm smootly hehe.

 

 

Reply
Yut
Yut
Leader

Posted: ‎2019-05-23 09:40 PM

0 Likes
1
9148
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
‎2019-05-23 09:40 PM

You can use the first PM8000 as gateway using ION protocol.

Reply
SESA528
SESA528 Contributor
Contributor

Posted: ‎2019-05-28 09:39 AM

0 Likes
0
9134
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
‎2019-05-28 09:39 AM

Hi @Yut ,

 

Thanks very much.

Reply
sarfraj
sarfraj
Explorer

Posted: ‎2024-05-04 01:57 AM

0 Likes
1
5741
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
‎2024-05-04 01:57 AM

How Can i change Parity Bit in PM8000 ?

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-05-06 11:57 AM

0 Likes
0
5731
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
‎2024-05-06 11:57 AM

Hello @sarfraj ,

 

This can be change from the front panel or software like ION Setup (https://www.se.com/us/en/download/document/ION_Setup_Latest_Release/)

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.