Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84606members
353882posts

Can we change the default telnet port number in ION meters?

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa101813_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
2
450

Can we change the default telnet port number in ION meters?

Hi Everyone,

Our customer is using ION8400,8600, 8650.

They are asking whether the default telnet port number can be changed to another number for their security.

Is it possible?

Best Regards,


Accepted Solutions
sesa64419
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
409

Re: Can we change the default telnet port number in ION meters?

Hello

You can change the Telnet port number on the ION8650 using ION Setup. You may need to update to the latest version of ION Setup and have recent ION8650 firmware loaded on your meter.

1. Connect to your meter using ION Setup

2. Open the Setup Assistant for your meter

3. Go to Communications > Network Settings and select the Protocols tab.

4. Select Telnet from the list and click Edit.

The Telnet protocol information is displayed. You can enable/disable and change the port number by entering a different number in the Port Number field.

This information is also on page 105 in the latest version of the ION8650 User guide, which can be downloaded from here:

http://www.schneider-electric.com/en/download/document/7EN02-0306-02/

Regards,

Alana

See Answer In Context

2 Replies 2
sesa64419
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
410

Re: Can we change the default telnet port number in ION meters?

Hello

You can change the Telnet port number on the ION8650 using ION Setup. You may need to update to the latest version of ION Setup and have recent ION8650 firmware loaded on your meter.

1. Connect to your meter using ION Setup

2. Open the Setup Assistant for your meter

3. Go to Communications > Network Settings and select the Protocols tab.

4. Select Telnet from the list and click Edit.

The Telnet protocol information is displayed. You can enable/disable and change the port number by entering a different number in the Port Number field.

This information is also on page 105 in the latest version of the ION8650 User guide, which can be downloaded from here:

http://www.schneider-electric.com/en/download/document/7EN02-0306-02/

Regards,

Alana

sesa101813_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
409

Re: Can we change the default telnet port number in ION meters?

Hello,

Thank you for your good information and quick reply!!