Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Can the TOU module be used in the PM8000 to enhance/replace the existing TOU calendar?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Can the TOU module be used in the PM8000 to enhance/replace the existing TOU calendar?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Anonymous user
Not applicable

Posted: ‎2015-12-04 08:26 AM

0 Likes
2
1478
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
‎2015-12-04 08:26 AM

Can the TOU module be used in the PM8000 to enhance/replace the existing TOU calendar?

The current TOU functionality in the PM8000 is pretty robust but doesn't meet the needs of every market. Is it possible to use the TOU module in PM8000 as a custom framework to either replace or enhance the existing TOU capabilities in the meter?

The specific application I have in mind is for Isreal (Moshe Maharaban, Yariv Enoch). They need to break down the TOU on Friday as they have two rate schedules on this day.

Thanks - Adam

Tags (4)
  • Tags:
  • custom_application
  • framework
  • pm8000
  • tou
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
sesa56307_bridg
sesa56307_bridg Troubleshooter
Troubleshooter

Posted: ‎2015-12-04 12:01 PM

1 Like
0
1440
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
‎2015-12-04 12:01 PM

The TOU schedule is highly configurable on the PM8000 (and other ION meters that support the TOU ION module).  I would encourage you to review the detailed description of the TOU Module in ION Reference, to see if it can be configured to meet the specific application you have in mind.  Here is a link:

http://download.schneider-electric.com/files?p_Reference=70002-0290-06&p_EnDocType=User%20guide&p_Fi...

From the basic description you gave, it sounds like there is a need to use a different rate schedule on Fridays, compared to other days of the week.  One possible approach would be to use the "Alt 1 Days" and "Alt 1 Rates" setup registers to specify an alternative rate schedule that applies to all Fridays.  This is similar to the example given in ION Reference which says:

"Alt 1 Days

This register defines a set of alternative dates for all seasons. These dates

generally have different rates from weekdays, weekends, or holidays (for example,

a company with a less expensive rate every Thursday). The rates in the Season 1-

4 Alt 1 Rates setup registers are used on these days."

You will need to assess the specifics of the application against the capabilities of the module, but given the configurability I expect a solution will likely be possible.  Some advanced configuration of the ION framework will be needed though, to make use of the additional rate information in measuring the relevant parameters.

Thanks,

Dave Tuckey, Firmware Architect

Reply
Yut
Yut
Leader

Posted: ‎2015-12-07 11:00 PM

0 Likes
0
1440
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
‎2015-12-07 11:00 PM

I think the TOU on ION meter is very flexible enough try to understand it well. In Thailand we can put holidays according to Lunar calendar which is updated every two years. If you think it not flexible enough you can use Friday status to control the Scheduler module as well.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.