Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

NERC compliancy on ION meters

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • NERC compliancy on ION meters
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
MatthewP
MatthewP Troubleshooter
Troubleshooter

Posted: ‎2015-12-03 01:05 PM

0 Likes
2
1229
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
‎2015-12-03 01:05 PM

NERC compliancy on ION meters

Referring the V4.20 firmware release notes for the ION8650

http://www.schneider-electric.us/documents/news/offer-news/schneider_electric_announces_powerlogic_i...

It mentions compliancy with NERC 5... "The ION 8650 meter V4.20 enables Utilities to comply with the latest NERC CIP standard Version 5, which is designed to protect the bulk power system against cybersecurity compromises that could lead to misoperation or instability. Utility Compliance represents significant progress in mitigating cyber risks to the grid."

I am currently working on project with a utility and numerous concerns around NERC compliancy have come up. From my understanding, NERC compliant devices must have the ability to be COMPLETELY locked down meaning that ZERO changes can be made to the device.

Can someone please provide technical details on how this has been implemented on the meter?

Will this be NERC compliance be available on the 7650/7550 platform as well?

Thank you!

Matthew

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Anonymous user
Not applicable

Posted: ‎2015-12-04 10:49 AM

0 Likes
0
1182
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
‎2015-12-04 10:49 AM

If I understand correctly you can disable front panel access, and turn off all ports and protocols for ethernet, as well as set all serial comms to protocol none.

Take a look at the comms modules in V4.20.1 you should see some new setup registers.  be careful though I think you can lock yourself out permanently.

Brian

Reply
sesa56307_bridg
sesa56307_bridg Troubleshooter
Troubleshooter

Posted: ‎2015-12-04 11:37 AM

1 Like
0
1182
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
‎2015-12-04 11:37 AM

In addition to the comments from Brian, I'd encourage you to review the "What’s new in PowerLogic ION8650 version 4.20 (v4.20)" document, which provides a short summary of the new security-related features and changes.  Here is a link:

http://download.schneider-electric.com/files?p_Reference=7EN12-0287-00&p_EnDocType=User%20guide&p_Fi...

Regarding NERC CIP in general, please note that this is a (large) set of standardized requirements that apply to an entire system, and the related features on the meter are intended to help our customers comply with these requirements.  Some of the requirements are related to workflow/process (for example, how often passwords need to be changed across the system), while others imply direct needs for features at the device level.  Some of the requirements were already met in previous firmware releases; the changes in V4.20 simply closed some notable gaps, making it easier for our customers to achieve NERC CIP compliance.

Matthew, if the customer you are working with still has some remaining concerns around NERC compliancy, please contact me separately as I would be interested to discuss the specific requirements of concern.  I'm not sure exactly which requirement relates to your example of completely locking down the device, although I think that the combination of HW locking, advanced security usernames/passwords, security settings like enabling/disabling ports and protocols, and auditability of any changes should be enough to satisfy them.

Thanks,

Dave Tuckey
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.