Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Can the PM8000 log the maximum KW value observed for the month and write those values to modbus registers going back to up 24 months?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Can the PM8000 log the maximum KW value observed for the month and write those values to modbus registers going back to up 24...
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
maks.chayun
maks.chayun Explorer
Explorer

Posted: ‎2025-07-10 07:40 AM

0 Likes
2
1252
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
‎2025-07-10 07:40 AM

Can the PM8000 log the maximum KW value observed for the month and write those values to modbus registers going back to up 24 months?

Hello!

 

Can the PM8000 series meter store the maximum KW value observed for the current calendar month and store the value within memory (that can be read as a modbus register) and recalled for the past 24 months before the current one as well? Tech support informed me that it is possible using custom max module, custom periodic timer module, and custom data recorder module on a daily basis that is triggered to reset at midnight each day, but can this done at the last day of a calendar month as well? Is there a way to make those valuables visible on the meter screen like the example I've provided in the attached picture (doesn't have to be this exact format)? How would it be done? 

Attachments
Labels
  • Labels:
  • ION Setup
  • PM Guidebooks
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-07-10 09:45 AM

1 Like
0
1241
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
‎2025-07-10 09:45 AM

Hi @maks.chayun 

 

Yes, the meter has a Clock module that can send pulses and trigger other modules at the end of each period, such as New Day, New Month, New Year, etc. Therefore, you can use the Clock module instead of the Periodic Timer module to reset the values at specific times.

Mehran_Mehrnia_0-1752165773560.png

 

You can link the desired values to the Custom Screen module to display them on the meter’s front panel.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-07-10 11:10 AM

1 Like
0
1230
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
‎2025-07-10 11:10 AM

Hello @maks.chayun ,

 

Note that values logged in data recorders are not visible from front panel. You could possibly make use of store modules that cascade to store the information in a way that can be accessed via the front panel. Note this is not retroactive and would only apply to months moving forward.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 2
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-07-10 09:45 AM

1 Like
0
1241
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
‎2025-07-10 09:45 AM

Hi @maks.chayun 

 

Yes, the meter has a Clock module that can send pulses and trigger other modules at the end of each period, such as New Day, New Month, New Year, etc. Therefore, you can use the Clock module instead of the Periodic Timer module to reset the values at specific times.

Mehran_Mehrnia_0-1752165773560.png

 

You can link the desired values to the Custom Screen module to display them on the meter’s front panel.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-07-10 11:10 AM

1 Like
0
1230
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
‎2025-07-10 11:10 AM

Hello @maks.chayun ,

 

Note that values logged in data recorders are not visible from front panel. You could possibly make use of store modules that cascade to store the information in a way that can be accessed via the front panel. Note this is not retroactive and would only apply to months moving forward.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.