Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hello Team,
Any experience with summing transformer ?
One of my customer wants to add summing transformer to connect to an energy counter.
Goal is to have one measurement point to have Power Delivered and Power Received (need a Modbus register to connect to a PLC in case of "Power Received" - no grid injection allowed).
Anyone has experienced this kind of config ?
Is it compatible with bidirectional power ?
Thanks for your help.
Link copied. Please paste this link to share this article on your social media post.
Hi,
If the loads distributed on the two lines are symmetrical and equal, this setup will work more reliably and accurately. All current transformers connected to the summation CT must be exactly the same type and rating.
If the loads are not equal, I would recommend using two separate energy analyzers instead of this method.
That said, your diagram is correct for equal system. Summation current transformers are typically used to combine signals from multiple CTs and to scale the output current to a level suitable for energy analyzers.
Link copied. Please paste this link to share this article on your social media post.
Hi,
If the loads distributed on the two lines are symmetrical and equal, this setup will work more reliably and accurately. All current transformers connected to the summation CT must be exactly the same type and rating.
If the loads are not equal, I would recommend using two separate energy analyzers instead of this method.
That said, your diagram is correct for equal system. Summation current transformers are typically used to combine signals from multiple CTs and to scale the output current to a level suitable for energy analyzers.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.