Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello, our customer has four SCADA systems that will consume data from ION Meters, and their pattern is to use different ports for each system.
I told them to use NAT on the routers, but they want to know if it's possible to bind/open different ports for IEC61850.
Is that possible? If so, how?
Thanks in advance.
Link copied. Please paste this link to share this article on your social media post.
Hello @Ezequiel-PROLUX
Is the customer wanting to have a different port for each IEC61850 connection, or have all the connections use the same port but on a different than default port?
Option 1 is not possible, the ports are on a per protocol settings and not that granular. Option 2 is possible on some meters with the latest firmware. You did not include what meters were were talking about nor the firmware so I could not say.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @Ezequiel-PROLUX
Is the customer wanting to have a different port for each IEC61850 connection, or have all the connections use the same port but on a different than default port?
Option 1 is not possible, the ports are on a per protocol settings and not that granular. Option 2 is possible on some meters with the latest firmware. You did not include what meters were were talking about nor the firmware so I could not say.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi Charles, is the option 1 that they want.
So this can only be achieved with routers configuration.
Thanks for your quick answer!
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.