Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84321members
353479posts

COM4 configuration error ION8650

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Miguel_Huaccha
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master

COM4 configuration error ION8650

Hello everyone,

I could help with this problem that I have ?; I want to configure a ION8650B COM4 meter so you can communicate with the communication protocol DNP3.0 but shower at the time of configuration I get this error?

Deputy screenshots taken from the error.

http://www.mediafire.com/view/63j20qas0656e15/Meter_Configuration_Report_for_MW-1406A170-01.txt

http://www.mediafire.com/download/3b3hdvq50ckag94/Error+ION8650.docx

Thank You

Miguel Huaccha


Accepted Solutions
Victor_Yacu
Lieutenant JG
Lieutenant JG

Re: COM4 configuration error ION8650

Hi Miguel,

You have to configure the "3rd Party Protocol" for this meter via ION Setup.

6965

In DNP3.0 option you have to set up "Connection #1" to "Communicaction port 4 (DNP V3.00)"

6966

Best Regards

Farid

See Answer In Context

1 Reply 1
Victor_Yacu
Lieutenant JG
Lieutenant JG

Re: COM4 configuration error ION8650

Hi Miguel,

You have to configure the "3rd Party Protocol" for this meter via ION Setup.

6965

In DNP3.0 option you have to set up "Connection #1" to "Communicaction port 4 (DNP V3.00)"

6966

Best Regards

Farid