Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84740members
354164posts

Automatic on-board logging export for ION7650/ION8650

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa300708
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
4
494

Automatic on-board logging export for ION7650/ION8650

Good day,

I read the user manual for ION7650 and ION8650. I didn't see an automatic export of data for ION7650 and ION8650 to a server.

I there any way that this is possible?

Thank you,

Josef

Tags (2)

Accepted Solutions
sesa64419
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Automatic on-board logging export for ION7650/ION8650

Hi Josef

You could use the Log Export module to send an email with logged data from either the ION7650 or the ION8650.

The Log Export module is described in the ION Reference, and you could create and configure the module using the advanced mode of ION Setup or through PME.

You can get the latest version of the ION Reference by searching "ION Reference" on the Schneider website.

cheers,

Alana

See Answer In Context

4 Replies 4
sesa300708
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
444

Re: Automatic on-board logging export for ION7650/ION8650

Is there any way that this is possible?

VictorMarincus
Sisko Sisko
Sisko
0 Likes
0
444

Re: Automatic on-board logging export for ION7650/ION8650

Hello Josef,

Once the meters are connected to a Power Monitoring Expert system, the on-board data will be downloaded automatically into a SQL Database and then read back/processed into the software.

Regards,

Victor

sesa64419
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Automatic on-board logging export for ION7650/ION8650

Hi Josef

You could use the Log Export module to send an email with logged data from either the ION7650 or the ION8650.

The Log Export module is described in the ION Reference, and you could create and configure the module using the advanced mode of ION Setup or through PME.

You can get the latest version of the ION Reference by searching "ION Reference" on the Schneider website.

cheers,

Alana

sesa300708
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
444

Re: Automatic on-board logging export for ION7650/ION8650

Thank you Alana and Victor.

Big help!