Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84426members
353620posts

Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

Solved
obscuresc
Ensign
Ensign
0 Likes
8
2861

Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Hi all,

 

I'm using the latest version (v1.3) of the Application_Addons Library that is available in 'Toolbox SE M17x' via Box.

Some of the functions are written with lower case syntax and a majority also neglect using semi-colons on 'THEN's.

 

While the lack of semi-colons do not cause compile-time errors in my environment, the lower case syntax does.

I've been maintaining consistent case so far and have the case sensitive option enabled in 'Project options->Code generation'.

 

Could this library be updated with this in mind?

 

Cheers,

Jack

 

 

 

 

 

Tags (1)

Accepted Solutions
PierpaoloA
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
2776

Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Hi Jack,

 

thanks for your feedback. We will take this into account for the next release.

 

@FedericoM FYI

 

Best regards,

Pierpaolo

See Answer In Context

Tags (1)
8 Replies 8
Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
1
2828

Hello Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Hello François, @sesa193656_brid : Could you please help?

 

Regards.

Rodrigo G. 


Industrial Automation Community manager

Tags (1)
sesa193656_brid
Cadet
Cadet
0 Likes
0
2825

Re: Hello Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

@PierpaoloA,: Hello Pierpaolo, can you ave a look at this request ? Thank you

Tags (1)
PierpaoloA
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
2777

Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Hi Jack,

 

thanks for your feedback. We will take this into account for the next release.

 

@FedericoM FYI

 

Best regards,

Pierpaolo

Tags (1)
FedericoM
Lieutenant Lieutenant
Lieutenant
0 Likes
4
2737

Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Hello Jack,

 

I've uploaded an updated version 1.3.1 on box.

Please let me know if it solved your issues.

 

Federico

 

@obscuresc @PierpaoloA 

Tags (1)
obscuresc
Ensign
Ensign
0 Likes
0
2722

Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Hi @FedericoM,

 

Didn't quite solve my issues; the functions in the BU2SI folder the ones I have issue with.

 

Cheers,

Jack

Tags (1)
KCWong
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
2
2679

Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Please send me the Box link. Thanks.

Tags (1)
obscuresc
Ensign
Ensign
0 Likes
1
2677

Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Tags (1)
KCWong
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
0
2675

Re: Multiple functions in Application_Addons Library (v1.3) are written for case insensitive environment

Thanks a lot.

Tags (1)