Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

MPM BACnet Integration

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • MPM BACnet Integration
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Cody_Failinger
    Cody_Failinger
  • DavidFisher
    DavidFisher
  • RobertAndriolo
    RobertAndriolo
  • CraigEl
    CraigEl
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
4871 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

MPM BACnet Integration

Picard Product_Support
‎2018-09-11 04:38 AM

Issue

How can objects of a SmartStruxure™ Lite network be made available as BACnet points to third party BACnet building management system (BMS)?

Product Line

EcoStruxure Building Operation

Environment

SmartStruxure Lite

BACnet

Cause

The BACnet protocol is always active, as long as the network cable is connected. However, two different BACnet options can be selected: IP or Ethernet. The default option is Ethernet and this will need to be changed if BACnet over IP is required.

Resolution

The BACnet protocol is always active, as long as the network cable is connected. However, two different BACnet options can be selected: IP or Ethernet. The default option is Ethernet.

  1. To verify or to change which BACnet protocol is currently in use, select the SmartStruxure Lite Manager that you want to configure from the left-side Network panel.
  2. Then choose the BACnet configuration list item.
  3. Define the Network Number (if the protocol selected is BACnet IP).

    Note:

    The Network number must be defined only on the monitor Manager. It shall be different then the Parent Network where the monitor is connected.

    A BACnet Device is uniquely located by a network number and a MAC address. Creating two or more B/IP networks, each with a unique network number, can be useful for limiting the propagation of local broadcast messages and for providing security by confining traffic to a particular geographic or logical area.

  4. Select the desired protocol type from the drop-down list between BACnet IP and BACnet Ethernet.

  5. Then choose an optional port number (if the protocol selected is BACnet IP). Default is 47808.

  6. Select the BACnet Priority of the BACnet write action of the SmartStruxure™ Lite's network monitor. Default is 10.

    Note:

    SmartStruxure™ Lite does not support BACnet Write Priority, per se. However, in Firmware version 2.4.x and newer, it is possible to assign the write priority for all SmartStruxure™ Lite BACnet points. Default value is 10, except if you upgrade a Manager using a version 2.3.x or older, BACnet priority will be 8, but can be changed.

  7. Click the Save button to apply the configuration changes.

  8. Click hit the Save All button to make the modifications permanent and reboot the Manager for the new options to enter into effect.

  9. Change the BACnet instance number of the Manager if required.

IMPORTANT

Each Manager must have a unique BACnet device instance number. A Manager device instance number can be changed by selecting the top-left icon inside the left-side Network panel.

Labels (1)
Labels:
  • EcoStruxure Building Expert
Tags (1)
  • Find more articles tagged with:
  • 14001
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.