Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84577members
353848posts

Does StruxureWare DCE have a disaster recovery solution

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

DCIM_Support
Picard
Picard
0 Likes
3
165

Does StruxureWare DCE have a disaster recovery solution

This question was originally posted on DCIM Support by Barry Patterson on 2019-02-28


Does DCE have a manual or standby solution for disaster recovery.  We have multiple data centers supported by one StruxureWare physical appliance. Could a DCE VM be used as a failover solution for the physical appliance. Can a full backup from the physical appliance be restored to a DCE VM having similar resource allocations (MEM, CPU, Storage) but different MAC, IP and Hostname.  Understood that similar licencing would need to be obtained for the DCE VM.

(CID:140709556)

3 Replies 3
DCIM_Support
Picard
Picard
0 Likes
0
165

Re: Does StruxureWare DCE have a disaster recovery solution

This comment was originally posted on DCIM Support by Christopherus Laurentius on 2019-03-01


Not from DCE itself.

If you are going to VM route, perhaps consider leveraging on the HA/FT or DR solution from VM itself to maintain DCE's availability?

Do set the DCE's VM  MAC address to be static, so it does not change when being moved around across hosts.

 

>>Can a full backup from the physical appliance be restored to a DCE VM having similar resource allocations (MEM, CPU, Storage) but different MAC, IP and Hostname.

 

Yes you can do so.

Do get the license key/passcodes of existing physical DCE and contact tech support with valid software support to have it reset so you can re-activate it against the DCE VM's mac address.

(CID:140709592)

DCIM_Support
Picard
Picard
0 Likes
0
165

Re: Does StruxureWare DCE have a disaster recovery solution

This comment was originally posted on DCIM Support by spezialist on 2019-04-01


Dear Barry Patterson,

Tell us, please, did you solve your question or not?

With respect.

(CID:141269245)

DCIM_Support
Picard
Picard
0 Likes
0
165

🔒 Closed

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.