Posted: 2020-07-05 04:33 PM . Last Modified: 2024-04-03 05:03 AM
DCE Failed to transmit Alert
Hi
I am having these error appear in DCE logs as follows
The destination IP was an old DCO connected to this DCE before it was decommissioned.
How can I remove these error from the logs?
Best Regards,
TJ
(CID:138810042)
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
Posted: 2020-07-05 04:33 PM . Last Modified: 2024-04-03 05:03 AM
Hi Tj,
there is no place in DCE to remove the posts to DCO. Likely this is causing no issue and if that’s the case should be ignored. If however you feel you must get rid of these, the only way I know to do it is to:
1: recreate the DCO server at the same IP address as before
2: add this DCE server as a remote server
3: verify DCO is receiving data
4: remove DCE as a remote server
5: get rid of your new DCO server.
Because DCO was simply shut down and the the servers were never told to stop communicating in this way, DCE will keep reaching out. I believe this will stop it.
Steve.
(CID:138810059)
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
Posted: 2020-07-05 04:33 PM . Last Modified: 2024-04-03 05:03 AM
Hi Steve,
Thanks for the reply.
I will try it out.
BR
TJ
(CID:138810068)
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
Posted: 2020-07-05 04:33 PM . Last Modified: 2023-10-22 01:16 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.