Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

How to integrate MPM SSL controller over Bacnet IP

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • How to integrate MPM SSL controller over Bacnet IP
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidChild
    DavidChild
  • DavidFisher
    DavidFisher
  • MaximeLaudren
    MaximeLaudren
  • CraigEl
    CraigEl
  • Cody_Failinger
    Cody_Failinger
  • Product_Support
    Product_Support
  • sesa346290_brid
    sesa346290_brid

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3143 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to integrate MPM SSL controller over Bacnet IP

Picard Product_Support
‎2018-09-10 10:20 AM

Last Updated: Lieutenant MaximeLaudren Lieutenant ‎2022-08-18 09:26 AM

Issue

Unable to monitor a SmartStruxure Lite MPM controller over a Building Management System using BACnet to an AX BMS

Product Line

EcoStruxure Building Expert

Environment

SmartStruxure Lite Multi-Purpose Manager (MPM)

Cause

Misconfiguration of BACnet settings on a MPM controller.

Resolution

Open Building Expert on the controller with a supported browser. In this example both the MPM controller and the BMS system are in the same IP subnet range.

  1. Highlight the Device's name e.g. SmartStruxure Controller and go to the Configuration tab.
  2. On Ethernet Settings (ETH1)
    • The IP address of the MPM controller must be in the same subnet IP range of the BMS IP address, but not the same IP address.
    • Netmask must be the same subnet on both controllers (MPM and BMS) e.g. 255.255.255.0, if not then a BBMD/Foreign Device needs to be used.
    • Gateway IP if used.
  3. On BACnet Settings (BAC1)
    • Network ID (171) used on the MPM controller must be different than the BMS network numbers used for BACnet MS/TP and BACnet IP
    • Set Protocol to BACnet IP
  4. Click on the upper-left icon (Save database to flash)2.png
  5. Important! Right-click on "SmartStruxure Controller" then on "Restart Controller," be patient.3.png
  6. On the BMS Jace AX, under BACnet network, click on Discover, uncheck all MPM Networks assigned within the MPM (if this facility is available in the BMS), in this example we have only one, it’s #171, refer to point 4. If you don't uncheck MPM network number, the devices will still discover but with duplicates. In this example, network #1 is the BMS IP network and needs to be checked. Network #300 is the BMS MS/TP network number, and has no impact on discovering the MPM as a BACnet device. Click OK.4.png
  7. Here’s the result of the discovery, all the objects we had at point 4. are shown.5.png
  8. Now add the Devices to the Database, then select one device (in this example the SE8600 is selected), click the Discover button, all objects we had in point 4. are now in AX. Add them to AX database.6.png
Labels (2)
Labels:
  • EcoStruxure Building Expert
  • EcoStruxure Building Operation
Tags (4)
  • Find more articles tagged with:
  • 19473
  • DavidChild19
  • lite
  • MaximeLaudren22
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.